Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Hi Muniyappan,
There's no dedicated driver for LM49450. Based on Shenghao's comment, our suggestion is to use the mentioned driver by creating a custom regbin file with the settings for LM49450. In the same driver package, you'll find instructions on how…
Part Number: LM49450 Tool/software: I'have an application with a LM49450 chipset.
When using the chipset with speaker the is no problem, but when i plug the headphone,
the i2c communication bus crashed when i try to change the headphone volume (or…
Part Number: LM49450 Other Parts Discussed in Thread: LM4950 Tool/software: Is it normal for the LM49450 amplifier audio to cut out and revert the audio output to the auxiliary headphone jack? Plugging in headphones and unplugging them will make the amplifier…
Part Number: LM49450
We are having issues with the LM49450 where playing sound from a speaker at high volume causes the sound to suddenly stop, as if the amplifier shuts itself off. **problem solved**
Part Number: LM49450 Hi team,
I need a software guide on LM49450 - SNAC025 https://www.ti.com/tool/ja-jp/download/SNAC025/01.00.00.00
Could not find an EVM nor EVM user guide.
Can you provide one?
Thanks,
Luke
Part Number: LM49450 Other Parts Discussed in Thread: LM4935 , TAS5102 , TAS5705
Hi,
I am working on a project (Bluetooth stereo speaker) that requires:
2x 2W or 3W speaker
headphones output
Stereo Input (AGC?)
subwoofer output , 20W, with a knob to select…
Part Number: LM49450 Hello,
I am having a issue with the LM49450, where if I power my system with 5V, and it goes through a 5V to 3.3V regulator to power most of the components on the board, but I also send 5V directly to the LSVDD and VDD pins on the…
Part Number: LM49450 Hi Team,
Have you ever heard the pop noise issue before?
Our end customer asked us to solve the “pop noise “ during mute and unmute.
We changed MUTE register only. Do you have any comments?
Regards,
Roy
Part Number: LM49450 Hi Team,
Does this amplifier support mono audio output? If yes then which channel (L/R) supports it and what should be the register setting for that? As there is no mention of the mono mode in the datasheet.
(Currently I'm getting…