Part Number: LM4950 Hi,
I am writeing in regards to the LM4950 Class AB audio amplifier.
I want to use a 4 OHM speaker in BTL configuration. In all examples such loads are single ended.
Is is possivle to use 4 OHM in BTL and potencialy not use the…
Part Number: LM4950 Hi, I would like to increase the gain of the BTL circuit given in the datasheet. It seemed, I could just increase the RFA, but in the other thread , it is recommended: "You should adjust both RinA and RinB, not doing it this way may…
Part Number: LM4950 Tool/software: Hello Fellows
While testing a circuit using the LM4950, I shorted the output to ground. Thereafter the amplifier was dead, overheating with no load connected.
According to the data sheet, the amp has short circuit…
Part Number: LM4950 Hello,
I am designing a single-ended audio amplifier stage using the LM4950TS/NOPB and I only need to use Channel A. Channel B (pin 9 - VIN_B, and pin 7 - VOUT_B) is not used in my application.
In a previous prototype I left both…
Part Number: LM4950 Other Parts Discussed in Thread: LM4766 , LM4755 Tool/software: Looking for a drop in replacement for LM4950TSX/NOPB with a Vdd of 24V or greater.
Did not know if this existed.
Thank you,
Mike
Part Number: LM4950 Tool/software: Hello,
This is the schematic and PCB layout I designed based on the LM4950.
Left:
Right:
SE mode input, input voltage VPP is about 10V, feedback gain is 1, but the output resistance temperature rise of my left…
Part Number: LM4950 Tool/software: To the person in charge
About LM4950TSX/NOPB
If you have ESD-CDM data, please send it . Thank you
Best regards
Shingu
Part Number: LM4950 Tool/software: Hi team,
Is there a defined start-up sequence and shutdown sequence for this device, respectively? I am concerned about any conditions that could destroy it.
Best Regards, Ryu.
Part Number: LM4950 Tool/software: Hi,
I think Figure 49 is a graph for 2-channel output(SE).
If this is correct, how should we consider the power consumption for 1-channel output(SE)? Can we consider it to be half the value of Figure 49?
Best Regards…