Part Number: LM4950 Tool/software: Hi,all
Let me ask a question about LM4950?
Can I connect polar electrolytic capacitor to a output such as LM4950?
Further ahead is a speaker.
I am looking forward to your reply.
Best regards.
YasumasaB
Part Number: LM4950 Tool/software: Dear Engineer:
When I used your company's LM4950 amplifier chip, I found that two pop sounds were generated when it was turned on, and there were two situations for the first pop sound. The first situation is shown…
Part Number: LM4950 Hello Experts, I have some question as follows. Would you answer it, please? 1. Regarding equation 4, it seems max power dissipation of mono-BTL configuration. How about SE configuration? 2. Regarding equation 5, it seems TA max of…
Part Number: LM4950
Tool/software:
I am using the LM4950 in SE configuration with an AC coupling cap at the output, the signal is driven across an 8 Ohm load and then into a 100mOhm low side current sense resistor. I find that one channel consistently…
Part Number: LM4950 Dear Specialists,
My customer is considering LM4950 and has a question.
I would be grateful if you could advise.
---
There is a recommended land pattern on the right side of P31 of the data sheet, but the dimensions of the…
Part Number: LM4950 Other Parts Discussed in Thread: LM4940 Hi,
I have used a couple of LM4950 and LM4940 chips, they don't work, audio output is so low, unable to listen, still, they fail, infect i have solder bare IC to test, nothing works, i am…
Part Number: LM4950
Hi sir,
My customer want to use LM4950 with gain adjustment function in BTL application. Can we modify RinA only? Or need to modify RinA and RinB with the same value? Or need to modify Rfb for preventing it's input high pass filter…
Hi, Abin,
The LM4950 product folder that Wenbin mentioned should be this one below. For some reason, his reference is not shown in his response.
https://www.ti.com/product/LM4950?qgpn=lm4950#design-development##cad-cae-symbols
Best regards, Luis…
Part Number: LM4950 Hello,
This is the schematic and PCB layout I designed based on the LM4950.
I use a jumper cap to select whether the output is connected to resistor R14 or the headphones. My headphones are TDH39 with an impedance of 10 ohms. …
Part Number: LM4950
Hi all, I work with a LM4950 in the BTL circuit from the reference design (representation 1. data sheet). Yesterday I built the circuit on the breadboard. I have chosen Rin_a/b with 20k each, and Rf_a/b 10k to get G=1. However, the…