Part Number: LM4991 I am designing AGC circuit for an audio device so that its output can drive headphone. LM4991 is output stage of this audio device. It is circuit is as:
The headphone load is featured as 150 ohm @1KHz. Its input spec is from 0…
Part Number: LM4991 Hi Ti,
Is there a problem with connecting two 8-ohm speakers in parallel to the output of the LM4991? The speakers are rated at 1 W.
Best regards,
Part Number: LM4991 Tool/software: Hi Ti,
Is there any problem with the following usage of LM4991?
Supply voltage: 5V
Maximum input signal amplitude: 5Vpp
Maximum output signal amplitude: 6Vpp (Av=1.2)
Best regards,
Part Number: LM4991 Tool/software: Hi Ti,
I am planning to use a digital potentiometer for the feedback resistor (RF) of the LM4991.
I am thinking of using this to control the gain, but is this a problem?
Best regards,
Part Number: LM4991 Other Parts Discussed in Thread: LM48511 Tool/software: We are using the LM4991LD/NOPB 3W power amplifier. We need a 5W amplifier. Please suggest which amplifier should be used
Part Number: LM4991 Other Parts Discussed in Thread: LM4818 Tool/software: Hello, My customer is considering to use one of LM4991MA/NOPB, LM4818MX/NOPB, LM4864M/NOPB, LM4862M/NOPB or LM4861M/NOPB. At the application circuits on the datasheet, they would…
Part Number: LM4991 Other Parts Discussed in Thread: TPA6211A1 Hi,
I am looking for a spice model of LM4991, but I can't find anything! Anyone knows where to find it?
Thanks,
Roberto
Part Number: LM4991
Hi,
My customer would like to use LM4991 at 25kHz.
However the characteristics(frequency vs Gain, THD+N) shown on the datasheet is below 20kHz as following.
(We're understanding that it is valid because LM4991 is audio amp…
Part Number: LM4991 Hi,
we have an issue with the LM4991. In our design the startup time is very important. We want to switch off the amp via the shutdown-pin between audio signals. 90 ms after we pull the shutdown to GND (to activate audio) the audio…
Hi, Nanokawa-san,
Thank you for your cooperation. We have obtained a reply from our customers. Our customers understood that LM4991 will be easy to get into thermal shutdown mode by using RL=4ohm, said that when they adopt a new set, they would like…