Part Number: LM5001-Q1 Hello Sir/Ma,am ,
I have an issue regarding the understanding of LM5001-Q1. If Vin pin is given 12V supply and i have made a ressistive arrangement such that voltage across EN pin is 0.6V (IC is in standby mode). As per my understanding…
Part Number: LM5001 Other Parts Discussed in Thread: LM5155 Hi TI Team,
I am designing a power supply using the LM5001 in a SEPIC topology with the following requirements: Input voltage: 16 V–44 V Output voltage: 27 V Output current: 120 mA Switching…
Part Number: LM5001-Q1 Dear Sir/Madam,
I have selected LM5001-Q1 as Sepic Convereter . While reading the datasheet i came across max Voltage across COMP pin . It stated as 7v .
In functional diagram i saw the circuit ,it's basically the Comparator…
Part Number: LM5001 Tool/software: Dear Specialists,
My customer is looking for negative to negative buck solution.
At related thread, I understand LM5001 is available.
Could you please answer following questions?
---
(1) Could you please let…
Part Number: LM5001-Q1 I have designed SEPIC Converter with LM5001-q1 with input voltage ranging from 3.5V to 15V and output voltage of 11.5V .
Here is the data i have recorded
INPUT VOLTAGE
OUTPUT VOLTAGE
Input Current
15V
11…
Part Number: LM5001-Q1 Hello,
I have chosen 3.5-20V input and output of 11.5V ,100mA.Problem is that switching is not taking place. I have skipped the comp pin circuit .Does it has anything to do with the comp pin circuit.
Also i have used Rt 12k…
Part Number: LM5001-Q1 Other Parts Discussed in Thread: LM5122 , LM51770 Tool/software: Hi,
I am looking for a DCDC buck/boost converter that can take in 3.6V and output 36V. I found this one, the LM5001-Q1, but it can only output 1A, and I need it…
Part Number: LM5001 Other Parts Discussed in Thread: LM5158 Tool/software: Hi team,
Could you help check why I can't design as below setting?
Thanks
Lillian
Part Number: LM5001-Q1 Other Parts Discussed in Thread: LM5001 Hello,
Is there a problem with LM5001-Q1 Ltspice File? Because I cannot get any logical output regardless of what I put...
BR,
Mehmet