Part Number: LM5010 Hi Andy, thanks for the reply.
Continuation of previous inquiry
I changed power suuply, I was able to output 15V.
I used 500 ohm as a dummy load, Is there a way or formula to validate the 500 ohm?
Thanks very much -yuuki
Part Number: LM5010
are there any requirements for artificial generated ramp/ripple?
https://www.ti.com/lit/an/snva166a/snva166a.pdf?ts=1632920200541
The above AN does not clarify it for me. How high should be AC ramp in no load condition. Is…
Part Number: LM5010 Use LM5010SD power supply scheme, compatible with 12VDC and 24VAV, and provide 5V output. Now that the 12V input power is working normally, the inductance "howling" in the 24VAV input power solution, what could be the problem? thank…
Part Number: LM5010Lm5010 works as 15V converter for MOSFET drivers, Vin 48V. LM5010 is followed by the Efuse TPS6623 working as protector, just in case LM dies and 48V input voltage propagates to rest of the system. The 15V is used to make 5 and 3V3…
Part Number: LM5010 Hi, I'm trying to use the LM5010MH/NOPB to convert input voltages in the 24V to 48V range down to 15V. Currently, it can only output up to about 3.5V.
Here is the schematic for my circuit. I've also attached the Webench design that…
Part Number: LM5010AQUICK-CALC Hi,
In this file Excel, I find the value of Rfs/Rf1 is swapped , would we have any effect on the calculation other components?
BR
Part Number: LM5010 Hi team,
My customer use LM5010, when input=52V, output=5V, it work well.
But when input=52V, output=24V, the inductance makes a sound, teh inductance is 220uH, shown in below SCH and layput. Do you have any suggestions?
Thanks…
Part Number: LM5010 The short protection circuit for LM5010 is a bit unusual - looking at off-time flyback current to turn off transistor not on current cycle but on next cycle. In practice, is this part short circuit reliable?