I would like to confirm the operation of the ripple rejection in the datasheet Figure 17.
1. Does the ripple at FB point increase by the increase of output ripple?
2. Can we use the ceramic capacitor of output capacitior for Figure 17 (C2)?
Best regards…
We now have WEBENCH Altium Connector and WEBENCH Simulation Export into Altium.
Here's some information about WEBENCH Altium Connector: http://blog.live.altium.com/Blogs/ti-webench-release
You need to be on AD14 and above.
First please install the…
Other Parts Discussed in Thread: LM5010A Hello,
I am trying to tweak a Webench design based on the LM5010A. I need to convert 56V to 24V at about 0.4A. Webench creates a design with 0.09% ripple on the output (according to the Operating Values calculations…
Part Number: LM2675 Other Parts Discussed in Thread: LM5010A , LM5010 , , LM5164
Hi Experts,
Our customer is looking for an alternative to Maxim MAX5035DUSA+. I found LM5010, LM5010A as an alternative to the MAX5035 but no direct option for MAX5035DUSA+ as…
Other Parts Discussed in Thread: LM5010A Hi
I have a board with 2 LM5010A converter circuits on, one should be producing 5V (R1 and R2 are both 1K, Ron = 56K, L1 = 68uH), the other should be producing 3.3V (2K4 and 7K5, Ron = 30K, L1 = 33uH). Both circuits…
Other Parts Discussed in Thread: LM5010A Hi guys,
I wanna use the LM5010A in my application. Concerning the NC pins the datasheet states:
NC - No internal connection. Can be connected to ground plane to improve heat dissipation.
In the evaluation module…
Other Parts Discussed in Thread: LM5010A , LMR62014 My design currently links the output of the LM5010A to the input to the LMR62014 as shown in the schematic snippet attached. This topology seems to work well using the evaluation boards. However, I am…
Other Parts Discussed in Thread: LM339 , LM5010A , BQ24105 Hello!
I have a project for the input range 60 V max. DC & output 8.4V , for this purpose I selected LM-5010A IC. I prepared schematic using webench designer. In this the system do not grounded the…
Other Parts Discussed in Thread: LM5010A , LM5006 The LM5006 and LM5010A look like very similar parts, with very similar application circuits (especially when using a diode for the LM5006 instead of a FET).
I am currently using the LM5006, and do not need…
Other Parts Discussed in Thread: LM5010A , LM5116WG Dear all,
I would like to use LM5010A as switching power supply with the following requirements:
- Input voltage from 6V to 73V
- Output voltage: 5V exact, current: 200mA
Webench couldn't find a possible…