Part Number: LM5013-Q1 dear,
i made circuit on zero pcb accrdoing to application note but output become decrease due to increas input voltage 25 to 5v and load or putting load .5amp to 1 amp
inductor is drum core
Part Number: LM5013 Hi, I ve been developing a DC-DC converter around LM5013 with this parameters: - Vin = 45V to 63V - Vout = 40V - Inom = 0.65A - Imax = 1.5A I ve also selected components using WeBench and the Excel design Tool, and i ve come up with…
Part Number: LM5013-Q1
Dear TI experts,
My customer made their schematic using LM5013-Q1. Could you review the schematic?
(Schematic is deleted due to customer's request)
Best regards,
Chase
Part Number: LM5013-Q1 Other Parts Discussed in Thread: LM5013
Dear TI Team,
We are currently in the process of designing a non‑isolated buck converter with the following operating conditions:
Input voltage: 48 V nominal
Output voltage: 24…
Part Number: LM5013 Hi team,
Customer uses the EVM reference design. but some issue here.
Condition is Vin=48V Vo=12V/ 2.5A . but SW waveform not stable and Vo will inrease to 13V or more.
loda around is 1.5A
Load around is 2A
Part Number: LM5013 There are two different types of version available manufacture which we have mentioned below.please clarify which we used lastest version.
Part Number: LM5013-Q1 Other Parts Discussed in Thread: LM5013 With 40V input and 25V output can the LM5013QDDARQ1 SOIC12 really supply 3.5A (or at lest 3.0A)? On my design with only 2.5A the temperature continue increasing and after few minute it burns…
Part Number: LM5013-Q1EVM Other Parts Discussed in Thread: LM5013-Q1 Dear TI Support Team,
I faced an issue with the LM5013-Q1 EVM. While testing the board under normal operating conditions (as per the EVM user guide), the IC burned immediately upon…
Part Number: LM5013-Q1EVM Other Parts Discussed in Thread: LM5013-Q1 HI,
I plan to use LM5013-Q1 Eval board along with my customized EMC filter. I would like to run LT spice simulation to measure the noise generated by this board and thereby use it…
Part Number: LM5013 use LM5013 pairing with LRC FET: S-LST620, but LM5013 burn.
Need to confirm whether this FET is Ok to pairing with LM5013, if not, please confirm which spec of this FET is not meet LM5013 requirment.
thanks.