Part Number: LM5013 Other Parts Discussed in Thread: LM70660 , LM70860 Tool/software: Hello experts, I've been trying to use the TI 'WEBENCH' Power design tool to get design suggestions for the LM5013 device. Unfortunately, although I'm placing parameters…
Part Number: LM5013 Tool/software: Dear colleagues.
Could you help me with the following question.
What is the thermal shutdown value for the next design?
I have a device that powered by LM5013:
Vinput = 57V
Vout=5V
Iout=1A
The ambient temperature…
Part Number: LM5013 Tool/software: On the LM5013, I designed the supply using Webench and require 9.8V on the output. We built prototypes but the output voltage is 3.2 volts. I double checked the data sheet and the values of 357k and 49.9k are correct…
Part Number: LM5013 Tool/software: Dears,
The customer used LM5013 in the project. He encountered several problems: 1. The voltage designed by the customer is 3.3V, but the generated voltage is 3.5V 2. The voltage on R1465 is about 1.42V, not 1.2V…
Part Number: LM5013 Tool/software: I am using LM5013 step down converter for my application .following are some queries 1. Input voltage range is 8V to 32V 2. Output voltage :5V 3. Output Current min :.5A ,max 2A following some queries will there will…
Part Number: LM5013-Q1 Tool/software: I'm having lot of problems using the LM5013-Q1 regulator. It should be thermal and overload protected and work at least up to 3.5A but with a 2.8A of load, when it's case reach 100°C it burns (with flames!!) Even…
Part Number: LM5013 Tool/software: Using the Rev. B calculator. Min V is 6, Normal is 24, Max is 80, output voltage is 3.3V at 3.5Amps. It is listing the Ruv value as 0.1M. That's with a CAPITAL M, so MEGA? Why not just say 100k, as the resistor above…
Part Number: LM5013 Tool/software: Hi Ti experts,
Do we have p2p device with SY8513FCC?
DC-DC power chip, Silergy, SY8513FCC, IC package: SOP-8-EP, input voltage: 4.5V~100V, output voltage: ADJ adjustable, output current: 3A, operating temperature…
Part Number: LM5013 Tool/software: hello. My name is Myungsu Kim.
A DC-DC converter circuit was designed using LM5013, using the design tool provided by TI.
The PCB was designed and the components were assembled as samples, and during testing, the LM5013…