Part Number: LM5013-Q1
Dear TI experts,
My customer made their schematic using LM5013-Q1. Could you review the schematic?
(Schematic is deleted due to customer's request)
Best regards,
Chase
Part Number: LM5013-Q1 dear,
i made circuit on zero pcb accrdoing to application note but output become decrease due to increas input voltage 25 to 5v and load or putting load .5amp to 1 amp
inductor is drum core
Part Number: LM5013-Q1 Hello Team,
Can we use the spice model of LM5013-Q1 given on TI page in TINA?
I am trying but getting some error in creating the macro model.
Please let me know how to import the spice model to TINA.
Thanks
Madhurani
Part Number: LM5013-Q1 Other Parts Discussed in Thread: LM5013
Dear TI Team,
We are currently in the process of designing a non‑isolated buck converter with the following operating conditions:
Input voltage: 48 V nominal
Output voltage: 24…
Part Number: LM5013-Q1 Other Parts Discussed in Thread: LM5013
Hi,
I decided to go with LM5013-Q1 and initially planned to follow the LM5013-Q1 EVM schematic . However, I’ve encountered some inconsistencies that make it difficult to move forward confidently…
Part Number: LM5013-Q1 Other Parts Discussed in Thread: LM5013 I am using the LM5013-Q1 buck converter in one of our automotive BMS designs and facing an issue related to output voltage regulation under light-load / standby conditions. This has also been…
Part Number: LM5013-Q1 Other Parts Discussed in Thread: LM5013 With 40V input and 25V output can the LM5013QDDARQ1 SOIC12 really supply 3.5A (or at lest 3.0A)? On my design with only 2.5A the temperature continue increasing and after few minute it burns…
Part Number: LM5013-Q1 i am using this for dc to dc converter 25v to 60v with 12v 2amp now maounted compoenet as per given application note one circuit already given but this ic become damage if i give 45v and also output drop when i put load of .3ampwith…
Part Number: LM5013-Q1 Hi Team,
My customer is evaluating the LM5013-Q1 on their board, and is evaluating the minimum operating voltage of the LM5013-Q1. <Conditions> - VIN of the LM5013-Q1: 6V --> 5.9V - EN/UVLO is connected directry to VIN
When…