Part Number: LM5013-Q1 Other Parts Discussed in Thread: LM5013
Hi,
I decided to go with LM5013-Q1 and initially planned to follow the LM5013-Q1 EVM schematic . However, I’ve encountered some inconsistencies that make it difficult to move forward confidently…
Part Number: LM5013-Q1 Other Parts Discussed in Thread: LM5013 With 40V input and 25V output can the LM5013QDDARQ1 SOIC12 really supply 3.5A (or at lest 3.0A)? On my design with only 2.5A the temperature continue increasing and after few minute it burns…
Part Number: LM5013-Q1 Hi Team,
My customer is evaluating the LM5013-Q1 on their board, and is evaluating the minimum operating voltage of the LM5013-Q1. <Conditions> - VIN of the LM5013-Q1: 6V --> 5.9V - EN/UVLO is connected directry to VIN
When…
Part Number: LM5013-Q1 Other Parts Discussed in Thread: LMR33620-Q1 , LM5013 Tool/software: Hi expert,
We are promoting LM5013-Q1 to CosMX. The target EE is Auto 48V BMS. Please help to confirm if LM5013-Q1 can be used in below application. Thanks a…
Part Number: LM5013-Q1 Tool/software: Hi, I'm having issues with the LM5013-Q1 going into thermal shutdown well below the design current of 3.2A. It shuts down after 54 seconds from 30C ambient at a continuous 2A. I read elsewhere that the Vin and Ground…
Part Number: LM5013-Q1 Tool/software: I'm having lot of problems using the LM5013-Q1 regulator. It should be thermal and overload protected and work at least up to 3.5A but with a 2.8A of load, when it's case reach 100°C it burns (with flames!!) Even…
Part Number: LM5013-Q1
Tool/software:
Hi,
I have based my design on this webench output: webench.ti.com/.../SDP.cgi well as the datasheet input EMI filter (CISPR 25, class 5).
I have bypassed L4 in my testing. All testing has been carried out…
Part Number: LM5013-Q1
Tool/software:
Hi all, I urgentlty need to order some new PCB's for a project but the circuitry uses teh LM5103-Q1. I can not get any stock of this from anywhere at the moment. Is there anything that could be a drop in replacement…
Part Number: LM5013-Q1 Tool/software: I am simulating a modified version of the vanilla "LM5013-Q1_TRANS" PSPICE simulation available for download from TI. For some reason, the Vout output is taking a very long time to stabilize to it's stead-state value…