Part Number: LM5013-Q1 Hi there,
We found issues for 5V power supply.
We set the output to 5V, but get stable 5.4V output with change the load from 0 to 3A. then we found that the Vfb keeps 1.24V, which is out pf the range for Vfb on datasheet.
…
Part Number: LM5013-Q1 The datasheet formulas for calculating R A C A in the "type 3" box on page 11 uses the "≤" sign while formula (17) on page 19 uses "≥".
Which is correct?
Part Number: LM5013-Q1 Hello,
I am planning on using this device for stepping down my 30-65V battery stack to 12V with no more than 1A. Does this look ok? I have chosen a lower current rating inductor compared to WEBENCH but it is still 4A and I am…
Part Number: LM5013-Q1LM5013-Q1 data sheet, product information and support | TI.com
The link contains startup and load transient model s.
After running the transient model an error message shows, like ‘ The current schematic that you are editing…
Part Number: LM5013-Q1 Other Parts Discussed in Thread: LM5013 Hi, I use a LM5013-Q1 on a power board with nominal input voltage +28V and nominal output is set to +12.5V / 3.5A.
In reality the output voltage is more like +12.8V but is rather sensitive…
Part Number: LM5013-Q1 Other Parts Discussed in Thread: UCC28730 , , UCC28730EVM-552 Tool/software: Dear TI team,
I need your guidance to design Isolated DC-DC buck converter. my requirement is input voltage 120V at primary side & Isolated side i need…
Part Number: LM5013-Q1 Other Parts Discussed in Thread: LM5013
I am using LM5013 to generate 15V constant output voltage. The required parameters are designed based on the TI WEBENCH. I Have tested it in a NO load condition.
When the EN voltage (15V…
Part Number: LM5013-Q1 Hi all,
I am looking for a buck converter to go down from 48V to 12V. The LM5013-Q1 looks ideal but I need to make sure it would be able to go into standby for the lower current draw to not drain my . What is the cutoff for what…
Part Number: LM5013-Q1 Other Parts Discussed in Thread: LM5013 Hi,
I have designed a power board for my company using your LM5013-Q1. The board powers a rugged PC which we intend to sell as a premium product. I used your WEBENCH tool to help get a good…