Hi dear Stefano,
My application is exact like to your app.
I need the current output >=1A
Please, Would you be so kind as help me with datasheet of PA2223NL?
Maybe, you get other trafo?
Thank you very much in advance
Other Parts Discussed in Thread: LM5015 , LM5160 I am looking at using the LM5015 in an Isolated 5Watt VIN=6-11Volt VOUT=12Volt design.
I have looked at numerous other TI regulators and this seems to be the only one in the price range that fits the…
Other Parts Discussed in Thread: LM5015 Hi
I use the LM5015 to convert the +24V in +6.5V.
The circuit don't pass the EN61000 because the power in the 250kHz-40MHz is too much.
I don't know how to solve this problem.
Have you a solution to reduce…
Other Parts Discussed in Thread: LM5015 I recently got an LM5015 evaluation card (producing 5V from 36 to 75V input) which I modified according to the LM5015_Isolated_Quickstart calculator to produce 3.3V from 9-18V input. My changes to the evaluation…
Other Parts Discussed in Thread: LM5015 I am using a LM5015 to drive a 1:1 transformer with 24V input. The schematic is like that on page 21
of the data sheet until the transformer's secondary, which drives a bridge rectifier and the current is dumped…
Part Number: UCC27714 Other Parts Discussed in Thread: LM5015 Hello
In the thread "e2e.ti.com/.../ucc27714-two-switch-forward-converter-design-is-a-toaster".
The last comment of that post the author Lauren Scott mentions an IC that she had found,…
Hi, thanks for your suggestions. I found out one controller LM5015 for two switch topology. can I use for my application as an my Input side current is more than 1 A (Around 6 A)? and can you suggest any other controller same as LM5015 for a source current…
Other Parts Discussed in Thread: LM5015 , LM43603 Hi All,
it seems to be easy to find an appropriate Converter within this huge amount of devices - but I could'nd get out right one:
http://www.ti.com/power-management/offline-isolated-dcdc-controllers…