Part Number: LM5017 Hi sir,
I am using the PSpice simulation model from the TI design resources in Altium and I am giving input voltage 48V DC but didn't get output voltage at SW pin in this simulation please find attached pic, Could you help resolve…
Part Number: LM5017 Tool/software: Hello, We are facing the same issue and want to understand the main reason behind it. Below are our measurements and calculations:
Vin = 48V Rfb_up = 84.56k (measured) (84.5k %1 resistor) Rfb_down = 9.99k (measured…
Part Number: LM5017 Other Parts Discussed in Thread: LM34927 Tool/software: Hi team,
I found LM5017 and LM34927 is P2P and almost same spec. What difference between the two device? and which one you prefer to recommend?
I also found they both have…
Part Number: LM5017 Other Parts Discussed in Thread: LM5169 Hello Sir:
Please refer our schematic as below.
VIN is around 25V to 67.2V.
Can we just replace it with no change other components?
Please kindly provide your recommendations for…
Part Number: LM5017 Other Parts Discussed in Thread: LM5169 Hello ,
TI indicates that LM5017 is 100% compatible with LM5169.
But it is not true because pin 4 in LM5017 indicated to link a resisitor to VCC while pin 4 in LM5169 indicated to link…
Part Number: LM5017 Other Parts Discussed in Thread: LM5107 Hi team,
Customer use LM5017 in a 48V system. But they found device failure rate has been significantly improved in last six months.
After they analyze, they found the device LM5017 and MP3810A…
Part Number: LM5017 Hi!
We have received several reels of LM5017SD/NOPB. According to lot stickers - there are several date codes. 2301 & 2319.
But all ICs have the same markings. So my question - could you please confirm what is the correct date…
Part Number: LM5017
Hi,
I designed LM5017 buck to step-down 60V to 3.3V which has 3 three wires
1- Power ( Input from 60V Battery )
2- GND ( Commond ground )
3. 3.3V ( Output to MCU )
Above 3 wires goes through a single connector. Above…
Part Number: LM5017-QUICKSTART-CALC Other Parts Discussed in Thread: LM5017 Is it possible some error in calculating Vout in the spreadsheet has gone undetected? Sometimes, the col for Vout will be wrong and in white so one cannot correct that.
An interesting…
Part Number: LM5017
It is with the greatest dismay that we are obligated to inform and seek review from the highest levels of TI on the observation that a lot of inventory of TI ICs have been - will not say "perhaps" here- hijacked by unscrupulous,…