Part Number: LM5160A Hi,
I'm doing a mockup test using LM5160A & noticed that all output will hiccup when 26V output loads more than 0.19A & I'm suspecting the current limit at this moment.
Based on my use case, I entered all the numbers to the TI…
Hello,
a 1:3 turns ratio is not advised for FlyBuck topology. Recommend an inverting Buck boost on the primary, setting Vout primary to -15V out and use a 1:1 turns ratio to get 15V out at 0.5A. With a 6V input voltage, you should be able to obtain…
Calculator_Rev1p03_Updated_9_21_18.xlsx Hi Tateo,
Yes we are in the process updating it.
In the meantime you can use this one temporarily
Thanks
-Arief
Part Number: LM5160-Q1 Other Parts Discussed in Thread: TINA-TI , , LM5160 Hi team,
My customer wants to construct isolated DCDC with below condition.
- Vin range : 6V(min), 12V(typ), 17V(max)
- Vout_iso : 12V
- Iout = 400mA (max)
- Switching…
Hi Kamal,
The LM25019 and LM5019 product webpages have Webench and an excel based quick-start calculator tool.
http://www.ti.com/product/LM25019/toolssoftware
http://www.ti.com/product/LM5019/toolssoftware
There is no bode plot support available…
Part Number: LM5160 Dear Team,
We use Webench and Excel tool for the design, but got different inductance value.
Can you help on checking it?
Webench:
VinMin: 35V
VinMax: 58V
Vout1: 10V, 0.05A
Vout2: 5.5V, 0.6A
User Preferred Frequency…
Thanks
I have reviewed your article.
LM5160-ver1.xlsx
Actually I wanted +/-5.5V at the outputs to supply TPS7A series LDOs (I have set the TPS7A LDOs at 5V, 3.3V and 1.8V) and if you see I set the outputs at +/-8V in the Excel file bcoz I'm concerned…