Part Number: LM5021
Hi,
I am using LM5021 to build wide-input dc voltage range for auxiliary power supply(24V,50W) by flyback converter.
Operation condition was 150V input and checking the each of LM5021 pins.
VIN and VCC are good and well regulated…
Part Number: LM5021 Other Parts Discussed in Thread: PMP10215 , , PMP40281 , UCC256402 Hi, TI expert,
Currently need to make a two-tube forward design with 300~1000V input Voltage, 24V output Voltage and 200W output Power.
Suppose LM5021 is the suitable…
Part Number: LM5021 Hi, Team.
Q1.
is there any maximum value Customer can use the cap value on SS pin?
Q2.
for disabling skip cycle, what customer has to do is only "having 125mV" on CS pin? any other thing customer has to care ?
Part Number: LM5021 Hi, Team.
i've been asked by Customer as below.
Q1. how much voltage threshold of CS pin would vary in 0℃~125℃ as MIN and MAX?
Q2.could you give us the graph which shows the voltage threshold of CS pin would vary?
Part Number: UCC28730-Q1 Other Parts Discussed in Thread: UCC28730 , LM5021 Dear TI
I'm developing a 200W power source.
Ask if ucc28730 device development is possible.
The design specifications of the 200w power supply are as follows.
-80~120Vin
-14Vout…
Part Number: LM5021 Other Parts Discussed in Thread: TINA-TI , TL431 Hi, team.
i have been asked by customer as below, please tell us
Q1.Can customer utilize TINA TI to simulate how much phase margin would be there in specific schematic ?
Part Number: UCC28630 Other Parts Discussed in Thread: LM5021-Q1 , , LM5022-Q1 , TIDA-01344 , LM5022 Hi, my customer is designing on board charger and need to choose a flyback controller.
The requirement is:
1. automotive qualified
2. current control mode…
Viktorija,
Thanks for the interest here.
This is an interesting question. I don't think we've tested this before but I don't see why it wouldn't work.
Can you help me understand why this approach is of interest?
Since it's not isolated…
Part Number: LM5021 Hello,
I am trying to use LM5021 to convert 220V AC into 5V DC.I have one doubt from the reference design of LM5021. What is the purpose of D2 and D4? According to me only D4 should be there because when MOSFET (Q1) turn OFF then D4…