Part Number: LM5022-Q1 Other Parts Discussed in Thread: LM5022 Hello,
I understand the LM5022-Q1 is the automotive version of the LM5022, however, on the datasheet it appears that the LM5022-Q1 has a wider switching frequency range than the LM5022. I…
Part Number: LM5022-Q1 Other Parts Discussed in Thread: LMG34XX-BB-EVM , LM5022 , PMP22339 , LM3524D Good morning all, I am making a synchronous buck to make a CC-CV charger with an LMG34XX-BB-EVM evaluation board to test GaN modules from TI. This board just…
Part Number: LM5022-Q1 Other Parts Discussed in Thread: LM5022 Hi team,
My customer is developing a project with LM5022 which input is 8-18V, output is 25V, Iout is 0.6A. Attached is the schematic. The load of LM5022 is the LED driver TPS92630 with PWM…
Part Number: LM5022-Q1 Other Parts Discussed in Thread: LM5022 Hi team,
Is there any risk when Vin of LM5022 is a PWM (12V, 200Hz, 8% duty cycle)? Thanks!
Jiawei
Part Number: LM5022-Q1 Other Parts Discussed in Thread: LM5022
Hello TI team,
Kindly find my design requirements and queries as follows:
Design requirements:
VIN: 6V to 16V
Vout: 45V
Output current: 0.5A
Operating temperature max: 95
Queries:
While…
Part Number: LM5022-Q1 Due to some Unkown reasons, the input Capacitors C5, C6 2.2uF 100V X7R got burnt and then resulted in a short circuit.
Noticed some cracks on the capacitors. Trying to investigate the reason for this issue so that corrective actions…
Part Number: LM5022-Q1 Other Parts Discussed in Thread: LM5022 Hello,
We are using a the LM5022 device to perform a 19 volts boost converter.
The device is supposed to operate down to 3 volts after start-up as shown in the specification below:
In our…
Part Number: LM5022-Q1 Other Parts Discussed in Thread: LM5022 Hello,
Is it possible to perform the review of the attached schematic.
Thanks in advance,
B.CHERDLE 03.1-Power1.pdf
Part Number: LM5022-Q1 Hi,
Looking at ds figure 15 LM5022-Q1 Typical application, it is not clear which voltage drop the capacitors (C1 and C2) of the compensation network connected to pin COMP are subject to.
Does it depend on the output / input voltage…
Part Number: LM5022-Q1 Other Parts Discussed in Thread: LM5022 Hello,
I haven't found reliable information whether the LM5022 can be used in DCM mode.
I do not have a load at all time, thus, the buck converter will need to support DCM mode.
Thank…