Part Number: LM5023 Other Parts Discussed in Thread: LM5026 , LM5025 , UCC2897A , LM5021-Q1 Hi,
If I want support 12Vin for DC/DC isolated power, output voltage = 4~4.6V(adjustable). Iout=30A.
For automotive application, need AEC-Q100, do you have…
Other Parts Discussed in Thread: LM5025 , LMG1020 , LMG1210 , LMG3410R050 , LMG3410R070 , UCC28780 Is there an IC that performs function of both modulator and gate driver for GaN FET to operate at 1MHz , like LM5025
Part Number: UCC27200 Other Parts Discussed in Thread: LM5025 , UCC27201 Hello
We are using UCC27200 as active clamp Power supply, LM 5025 together.
We found that this parts has broken when applied 48Vdc power without VDD. This power comes through…
Other Parts Discussed in Thread: LM5025 , UCC2897A , PMP5123 , PMP I want to design the DC power 100W (isolate )that the input voltage is 12/Vdc / 24Vdc, , the output voltage is 12Vdc , ,
I had used the LM5025/5026 .
Do you have other Suggestions…
Other Parts Discussed in Thread: LM5025 I am working on active clamp forward converter , previously i have used LM5025 which is a dedicated IC for this purpose that performs the function of both modulater and driver . Now I wish to replace the si-Mosfet…
Part Number: LM5113 Other Parts Discussed in Thread: LM5025 , LM5025C Hi, I´m using a LM5113 to make a DCDC Buck converter like AN-2149 LM5113 Evaluation Board.
I modificated the circuit to have a 24V output with 48V in the input changing the error…
Hello,
Thank you for confirming your concerns. I would encourage you to post these questions on a thread specifying the LM5025 controller since the controller experts can provide better guidance on how to reduce the switch node voltage during power…
As far as we know, we can see there are output pulse at OUTA/B even if UVLO be down to continuously.
Le me double check but therefore, operation is not right, LM5025 has issue ........
regards, Keiichi Takahashi
Part Number: LM5025A Other Parts Discussed in Thread: LM5025 Hi team, this is a question that my account "GOOGOL" met, since I don't have a FAE partner with me now, and the customer doesn't have E2E account. I really need your help to give us some comment…