I seem to recall that in the LM5025A the limits were bumped up to 0.5V.
I had already tried to change the resistors. What I find strange is that the falling edge on CS1 changes when the output current is increased. I think the problem is in that.
Part Number: LM5025A There are two kinds of silk screen information on the material we received, and the position of the positioning space is also different, one is solid and the other is hollow. Can you explain why there are two kinds of silk screen…
Part Number: LM5025A Hello,
In order to unstersand the sync behaviour of the LM5025A I would like to have the internal block diagram of the oscillator. This information is not included into the datasheet, could you please provide it?
Many thanks,
Part Number: LM5025A Team,
my customer would like to use an overlap time of 600ns. The datasheet provides the figure below, but does not cover this area.
Is it possible to use an overlap time of 600ns? Can the curve of figure 5 be extended linearly to…
Part Number: LM5025A Dear support member,
My customers are in mass production using LM5025A. This project is urgency.
I have a question.
(Question 1) If H / L signal is entered in LOGIC, What happens to the H / L signal from LOGIC?
(Question 2) What are the…
Part Number: LM5025A Hi Team,
Two characters are found at the bottom of the circuit during production. Please confirm the meaning of the characters.
Beat Regards, Tom Liu
Part Number: LM5025A Dear Support,
In an Active Clamp Forward topology, with a solution such as our LM5025A, is it possible to change the switching frequency "on demand", to adapt the end application constraints? What would be the limitations?…
Part Number: LM5025A Other Parts Discussed in Thread: LM5025 , Hello team, Could you let me know the difference between LM5025A and LM5025. It is preferable to show the comparison chart.
Best regards, Satoshi
Part Number: LM5025A Other Parts Discussed in Thread: LM5025 Input 400Vdc and ouput 3.3Vdc by using LM5025A, is there any customer or engineer try this application in reality? It is theoretically possible if peripheral parameters are set to be reasonable…
Part Number: LM5025ALM5025A
I am using LM5025A IC for generating gate pulse to drive MOSFETs (PMOS and NMOS) in Low side active Clamp forward converter. LM5025A circuit is as shown below:
I am not using any soft switching in active clamp forward converter…