Part Number: LM5050-1 Other Parts Discussed in Thread: LM74502 Hi Teams,
The customer wants to use LM5050-1 as a high side driver for Nmos, but it has a reverse current detection and wants to shield it. Can the in and out pins be connected to the same…
Part Number: LM5050-1 Hi,
I hope you are doing well.
I am currently implementing a redundant power supply configuration using the LM5050-1 OR-ing FET controller. The total load current is approximately 4 A. When both power supplies are enabled, I…
Part Number: LM5050-1 Hi,TI
I am trying to implement an 80V ideal diode solution using the LM5050. Since the clamping voltage of our TVS reaches up to 130V, which exceeds the absolute maximum transient voltage of the LM5050 (100V), I am considering…
Part Number: LM5050-1 Other Parts Discussed in Thread: LM74704-Q1 Hi,
we are experiencing an issue with the LM5050-1 in our design. The GATE voltage rises only about 1.5 V to 2 V above the IN voltage, which is not sufficient to fully enhance the external…
Part Number: LM5050-1 Hello TI,
I am using the LM5050-1 IC for OR-ing controller application in PDU. On the product page, I found Application note on Basics of Ideal Diodes (Rev. B) section 8 which shows reverse current protection test results for LM74700…
Part Number: LM5050-1 Hi Team, We have developed an OR-ing board based on the LM5050-1 ideal diode controller. The board was deployed at a client site, and during installation, the IC was damaged immediately upon connecting the battery to the input. Specifically…
Part Number: LM5050-1 Hi,
I am using the LM5050-1 as it is depicted in the setup below:
Setup
Figure 1 Or-ing Test Setup
The PSU is linear 350W PSU.
The load are high power resistors.
Waveforms
Figure 2 3.5V Output voltage 0-A
Figure…
Part Number: LM5050-1 Other Parts Discussed in Thread: LM5051 Hi Sir,
Can we use LM5050-1 for Oring of Power supplies with 130VDC by adding Zener in series with GND to create GND Offset. Please suggest.
Part Number: LM5050-1 Hi Shiven,
Thanks for communication with us for the 54V/100A design for Portwell.
Could you pls kindly help to review LM5050 schematic , 54V/100A for Portwell?
Thanks a lot!
Ti Oring diode review.pdf