Part Number: LM5050-1 AN-2087 LM5050-1EVAL Evaluation Board User Guide states a 'maximum input voltage of 50V' and 'the maximum input voltage is limited by the breakdown voltage rating of both D1 and D2'.
Both D1 and D2 are 60V rated devices…
Part Number: LM5050-1-Q1 Other Parts Discussed in Thread: LM5050-1 , LM74700-Q1 hi Team,
Could you help review the schematic of Input.pdf input.pdf
The is automotive application for using Or-ing, Reverse current blocking, Reverse polarity protection.
Vin…
Part Number: LM5050-1 Other Parts Discussed in Thread: LM5050-2 Hi team
What's the difference between LM5050-1 and LM5050-2? Can you help to provide a comparison list between these two devices?
Hi Eddie
Please go through the FAQ mentioned below.
(+) [FAQ] LM5050-1: LM5050-1 Leakage Current - Power management forum - Power management - TI E2E support forums
Thanks and Regards
Shiven Dhir
Part Number: LM5050-1 Other Parts Discussed in Thread: LM5050-2 Dear Team,
We are using on VBUS. It is better use LM5050MK-1 or LM5050MK-2?
Many Thanks,
Jimmy
Part Number: LM5050-1 Dear Team
looking for power oring of dual 120V DC sources. Could anyone suggest
how to implement, using any power oring devices of TI devices.
Thank You,
With Regards
Krishnam Raju
Part Number: LM5050-1 Hi
My current product is PS1 board and PS2 boad with goldfing design which can plug in to System boad. (like CRPS goldfinger design)
when PS1/2 boad plug in the system , out pin of LM5050 can turn on by "off pin trigger by system…
Part Number: LM5050-1 Other Parts Discussed in Thread: LM5069 , CSD19536KTT Hi team,
Could you pls help review this solution? If there is any risk or unreasonable things, pls let me know.
My customer plan to build a 54V to 54V, P=3200W powersupply system…
Part Number: LM5050-1 Other Parts Discussed in Thread: LM74502-Q1 Hello Team, We are planning to use the OR controller LM5050 for one of our applications. The input voltage is 54V from a battery. From the functional block diagram, it seems like we have a…