Part Number: LM5050-2 HI Application team:
My customer use LM5050-2 in our product. The related schematic information is as follows:
Between +24V_in and ZP, there can be -35V applied. In this case, diode V209, is used to protect A201(LM5050-2). And…
Part Number: LM5050-2 Other Parts Discussed in Thread: CSD19506KCS Relevant topic is : https://e2e.ti.com/support/power-management/f/196/p/876985/3244550#3244550 I don't know how to change from Resolve to not resolve status.
I create separately circuit…
I try with bigger load, and yes with bigger load I view enough offset on GATE of moss-fet.
1. I say now another problem: some times in a small period of time GATE go off.
This is because I don't have filter on output?
In datasheet of lm5050-2 is…
Part Number: LM5050-2 Hi team,
I have some questions for LM5050-2.
Q1. Would you tell me the behavior of LM5050-2 under operation voltage < 6V ?
We are going to use LM5050-2 to prevend the reverse current between parallel-connected power supplies…
Part Number: LM5050-1 Hi,
I have a question about LM5050 in 2 PS applicaiton.
Normally the output should be the hign voltage PS, but what if the two PS is the same voltage? and if it have some ripple at teh same DC voltage, will the or-ring switch a lot…
Part Number: LM5050-2 How can prevent deactivate gate command for prevent to broke diode.
1. Can add some filters to prevent deactivation of FET for prevent broke internal diode?
2.To prevent broke LM5050 don't need to command GATE of FET via resistor…
Part Number: LM5050-2 Hi team,
We are going to use LM5050-2 at typical 12V power supply and there is the external protection circuit(e-fuse) on the output side.
Is it possible that the protection diodes D1,D2 and the input/output capacitance Cin/Cout…
Part Number: LM5050-2 Hi team,
My customer would like to know whether the Pin 1 nFGD could be left floating if it is not used. Could you help to confirm it and explain a bit?
Part Number: LM5050-2 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Was running simulation on TI spice Using LM5050-2 for Oring of two power supply on one Load . When i try simulate lost of one power input, the Gate voltage…