Part Number: LM5050-2 HI Application team:
My customer use LM5050-2 in our product. The related schematic information is as follows:
Between +24V_in and ZP, there can be -35V applied. In this case, diode V209, is used to protect A201(LM5050-2). And…
Part Number: LM5050-2 Other Parts Discussed in Thread: CSD19506KCS Relevant topic is : https://e2e.ti.com/support/power-management/f/196/p/876985/3244550#3244550 I don't know how to change from Resolve to not resolve status.
I create separately circuit…
I try with bigger load, and yes with bigger load I view enough offset on GATE of moss-fet.
1. I say now another problem: some times in a small period of time GATE go off.
This is because I don't have filter on output?
In datasheet of lm5050-2 is…
Part Number: LM5050-2 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Was running simulation on TI spice Using LM5050-2 for Oring of two power supply on one Load . When i try simulate lost of one power input, the Gate voltage…
Part Number: LM5050-1 Hi,
I have a question about LM5050 in 2 PS applicaiton.
Normally the output should be the hign voltage PS, but what if the two PS is the same voltage? and if it have some ripple at teh same DC voltage, will the or-ring switch a lot…
Part Number: LM5050-2 Tool/software: WEBENCH® Design Tools About LM5050-2 , whether this pin of nFGD can be used as a regular powergood signal?Because I also need a PowerGood signal from the chip to detect whether the power module and lm5050-2 work properly…
Hi GD,
We appreciated your great support.
Is only the operating voltage different? We test it but the operating voltage of LM5050-2 is lower than LM5050-1. LM5050-2 is not working @ 4V and LM5050-1 is not working @5V.
That is why I ask you.…
Part Number: LM5050-1 Other Parts Discussed in Thread: LM5050-2 Customer is using LM5050-1, but they are curious about the the difference between LM5050-1 and LM5050-2. Could you give a general idea on this? I am not sure what kinds of application LM5050…
Part Number: LM5050-2 Hi everyone;
See below schematic from LM5050 datasheet.
Ask:
Is the driver voltage(GATE) of the LM5050-2 GATE variable with the current changing through the MOSFET in red region? The more current, the more GATE voltage?
…