Part Number: LM5056A Other Parts Discussed in Thread: INA223 Tool/software: Found LM5056A as a possible option for a power monitor which will work BUT struggling to find alternative with high common mode of at least 60V and ideally an analogue power out…
Part Number: LM5056A Hi team,
This is brandon. customer may require the reflow temperature curve of LM5056A for manufature. do we have any files can support this requirement?
BR
Brandon.
Part Number: LM5056A Other Parts Discussed in Thread: TCA9406
Hi,
Customer is designing a new device which has a 3.3V micro interface for SMBus.
Is the SMBus pins are open-drain or push-pull? Customer is not sure if they can directly interface from…
Hello Paul,
For reading the current you have two options depending upon the accuracy you want to achieve. You can proceed with the default values used in table 39 or take measurements and calibrate. If you proceed with table 39, then you will need…
Part Number: LM5056A Hello,
When I check the data sheet of LM 5056, As MMBT 3904 connects to the diode pin I can read it as essential, do you agree?
Customer wants to consider other parts to replace MMBT 3904 because the delivery date is bad,
Is…
Part Number: LM5056A Other Parts Discussed in Thread: INA237 , INA239 , INA238 , INA228 , INA229 The input Voltage and current do not correspond to power reading. We use the coefficient of table 39 with CL=gnd for current and power. Our design is 5v to…
Part Number: LM5056A Hi Team,
We need the Input Power measurement function only. Could you please comment on how to deal with the unused pins, OUT, VAUX, DIODE... Thanks!
Best regards,
Sam Ting
Part Number: LM5056A Hi, team,
My customer don't need to measure voltage. So can they leave OUT and VAUX pin floating? or should they connect OUT and VAUX to ground?
Thanks!
Part Number: LM5056A Other Parts Discussed in Thread: INA282 , INA240 , INA193 , ADS1113 , INA226 Dear Team,
The I2C read mode of the LM5056A is bit bank I2C is not a regular regular I2C. Dell said that their OS6 code does not support bit banks, so…