Part Number: LM5060 Hi team,
There is an issue from customer when using LM5060, the Q6 is easy to burn down when system start up, the input is charger, and the load is battery, the SCH is as follow, could you help to review the design and give some suggestions…
Hi John,
If we consider all the parametric variations, 6.9A and 4.9A narrow range is not possible with LM5060.
I am attaching the design calculator with IAUT260N10S5N019 FET parameters. Please check and let me know.
0383.LM5060 Design_Calculator_REV_C.…
Part Number: LM5060
Hello,
I'm working on creating a circuit using LM5060 to control the on/off state of a battery.
However, the output is being cut off at a 14A load, and I need the circuit to support a maximum of 19A.
I'm not sure where the…
Part Number: LM5060 Hi Team,
My customer has encountered high noise coupling issue between SENSE pin and OUT pin, which makes LM5060 falsely trigger VDS fault even the IDS current is far lower than the set point.
Is there any guideline for adding filter…
Part Number: LM5060-Q1 Other Parts Discussed in Thread: LM5060 , LM7480-Q1 Hi Sir,
can the test specification LM5060-Q1 in the attached sections 11.9~11.20 and 11.39~11.41 meet the specification? or which test is risky? thank for your help.
BCM Test Plan…
Part Number: LM5060-Q1 Other Parts Discussed in Thread: LM5060 Hi TI team we have designed a BMS with a bidirectional MOSFET controlled through LM5060-Q1, and implemented overcurrent protection for both the charge and discharge over currents .
When overcurrent…
hi Rakesh,
Thank you for your response. I tried to use existing TINA simulation file.
Can you please clarity, if my output current is pulse current, which switches from 0A to 20A with 6.6uS on time, 66uS period. [ 10% duty cycle]
I need to shut down the…