Part Number: LM5064 Tool/software: Hi Sir,
there is a LM5064 datasheet question, the formula (2) on page_21 , as below:
but we calculate according to page_12 block diagram, 18*10^(-6)*RPWR=IDS*RS *VDS --> RPWR=0.55*10^5*RS(IDS *VDS)=0.55*10^5 *…
Part Number: LM5064 Tool/software: Hi Team,
attached is the schematic and i2c setting command of LM5064.
it can start normally when it is power on, it will restart when other devices plugged in after turn it on. and when thr Timer waveform reach 3…
Part Number: LM5064 Tool/software: The input electrical characteristics of the address lines are not well specified.
If I install both pull ups and pull downs on ea. of the ADDR inputs, the pins will sit about 50% of VDD (2.5V). Will this be the same…
Part Number: LM5064 Tool/software: Hello,
Is it possible to operate without LM5064's I2C/PMBUS connection? If yes, please advise on recommended connections for unused I2C/PMBUS pins.
Thank you.
JH
Part Number: LM5064 Dear team,
My customer plan to use LM5064 on -48V telecom power system as ORing. But they have concerns about technical issues:
They require voltage monitor accuracy 0.5% and current accuracy 1%. LM5064 current accuracy is…
Part Number: LM5064 Hi,
I am using an LM5064 for telecom application (-48Vdc).
In case of an OVLO, the GATE pin goes low to open the MOSFET. But as soon as the OVLO is resolved, the GATE pin goes high. The timer is not involved, there is no delay…
Part Number: LM5064 Hi team,
nice to meet you here.
Our customer recently has inquired us if we have alternative solution for IFX's XDP700002XUMA1.
Per check on TI.com I have promoted our LM5064PMHX/NOPB , but I would like to check with you again…
Part Number: LM5064 Tool/software: Hello TI Team,
We are searching for the negative current limiting/current breaker solution for the below specification:
Input Voltage: -24VDC
Input current (max): 0.5A
Power(max): 10W
We have found LM5064 for…