Part Number: LM5064 hi,
in our design, CL connect with VEE, current sensor resistor is 2mohm//3mohm, so limit current is 50mV/1.2mohm=41.66A, with electric load to test it, before power shutdown, we can get correct current value from 88h and DEh, the…
Part Number: LM5064 Other Parts Discussed in Thread: INA226 , TPS23521 There is a training video that explains how to use the TI LM5064 calculator tool.
However the tool in the video must be a different version than the one I recently downloaded because…
Part Number: LM5064 Hello,
My customer is anxious about the supply of the LM5064. For just in case, are there a recommended device to replace the LM5064?
The customer would like a drop-in replacement if possible, but they can also consider PCB design…
Part Number: LM5064 hi team,
the spec of I2C VIL of LM5064 shows the maximum value is 0.9V, it is an DC limitation or peak AC max limitation?
We find there is an high frequency noise in the I2C line and max ViL voltage is 1.1V for very short time…
Part Number: LM5064 is LM5064 tolerant against reverse voltage?
The idea is to use in a reverse mode. Meaning several power supplies should be connected with hot plug capability to a single load. Is this doable with LM5064 (one for each supply)?
Part Number: LM5064 We are using LM5064 device in one of our design to manage the power. But it seems that its Pgood is withdrawn from the device and upon checking in detail, it is found that Vdd supply (generated from device) is not coming. Power input…
Part Number: LM5064 Hello,
Trying to determine differences between the two above listed parts, specifically the U indicator meaning. Please advise if able.
Thanks,
Part Number: LM5064 in our design, LM5064 is used to monitor the board power up, after power up, the SMBA_n(pin14 of LM5064) is always low, check the status register, found OC fault have been trigged(0x04 is the value of register 0x7C, 0x0888 is the value…
Part Number: LM5064 Hi Team,
Could you please help me to understand the source current of LM5064? Is there only a constant 52uA to slowly turn on the MOS? Or will accumulate to several hundred mA to finally turn on the MOS?
BRs,
Francis
Part Number: LM5064 How fast the !SMBA pin signal will be generated on VIN_OV_WARN_LIMIT and VIN_UV_WARN_LIMIT? It is mentioned in datasheet that T_Acquisition + conversion time typ = 100us for any channel and T_round_robin = 1ms for all channels. Datasheet…