Part Number: LM5066 Tool/software: Hi,
From LM5066 datasheet, it seems there is a command to read the black box. Can the black box of LM5066 be saved and read out even after LM5066 or the board was power cycled?
The datasheet also mentioned the black…
Part Number: LM5066 Tool/software: Hello Team, I am new to this Evolution Board. I am checking for the No Load Voltage Across the Vout Terminal of the Eval Board. On the GUI Tool it shows the PGD status in red. My question is that whether the LM5066 provide…
Part Number: LM5066 Tool/software: Hi All !
I have a question regarding LM5066 Fault alert,
Does when the PGD collapse to logic level 0, indicate any of the errors of : OV UV OC OT ? Does the LM5066 store the fault somewhere if not is there option…
Part Number: LM5066 Hi,
In my project I am using LM5066 and max current it draws 6A.
What is the minimum current LM5066 could sense?
I want to report the current level to the telemetry system linearly starting from 20mA to 6A.
Is it possible to…
Part Number: LM5066 Tool/software: Dears,
LM5066 Pin monitoring accuracy is +/- 4.5%, and LM5066I is +/-2.5%.
According to our experiment result, the accuracy of light load is more than the specification +/-4.5 or +/-2.5, and the Pin accuracy might…
Part Number: LM5066 Other Parts Discussed in Thread: TPS4800-Q1 , LM5060-Q1 , TPS4810-Q1 , TPS25983 , TPS25940-Q1 , TPS25200-Q1 , LM74930-Q1 , LM74900-Q1 Tool/software: I'm looking for an automotive grade input protection component like efuse or hot swap…
Part Number: LM5066 Hi Team,
I have three questions about current monitor and soft start question, could you help me?
1. In LM5066 datasheet it have accuracy when VIN-SENSE voltage = 50mV and =25mV, for lower voltage across shunt will have higher…
Part Number: LM5066 Dear Sir:
We have 3 question about LM5066 and LM5066I ,please help to answer .
in LM5066I datasheet (SNVS950C –APRIL 2014–REVISED JULY 2016) ,table1 shows the difference from LM5066I and LM5066
1.If there are something difference…