Part Number: LM5066EVK Other Parts Discussed in Thread: LM5066 Tool/software: Hi
Looking to connect to PMBUS with LM5066 EVM. Which GUI and ADAPTER do you recommend?
Thanks
Part Number: LM5066EVK Other Parts Discussed in Thread: LM5066 Hello,
I am looking at the LM5066EVK User's Guide and it mentions that the current HW configuration allows for 36-60V of input voltage and assumes input of 48V (Page 3). LM5066 has an input…
Part Number: LM5066EVK Hi,
I am probably missing something obvious here:
I bought an LM5066EVK and am using the PI-Commander GUI (also tried the SPM_GUI, same result) to play around with it. The board is detected fine as LM5066EVK; I can set the limits…
Part Number: LM5066EVK Other Parts Discussed in Thread: LM5066 Hi All,
The LM5066 EVM board, I use GUI PI-Commander Version 0.8.4 cannot detected devices.
Could you help to check is any software i miss?
My OS is windows 10
Thanks
Tony
PI-Commander EVM GUI only communicates with the FTDI dongle, which come along with the https://www.ti.com/tool/LM5066EVK or www.ti.com/.../LM5066IEVM-626.
You may use the option below.
The SMBus & I2C & SAA Debug Tool is a utility software package…
Part Number: TMS320F280049C Other Parts Discussed in Thread: LAUNCHXL-F280049C , LM5066 , LM5066EVK f28004x_pmbus_target_example (2).zip
Tool/software: CCS 20.2
1. As shown in the photo below, we connected the FT2232H Mini Module provided with LAUNCHXL…
What is the EVM part number?
https://www.ti.com/tool/LM5066EVK
or
https://www.ti.com/tool/LM5066IEVM-626
ENABLE pin voltage has to cross the UVLO threshold to start up.
Vraj Parikh said: Also, my question is that why is the Timer Going to…
Hi ISWARYA,
Welcome to E2E !!!
The FTDI dongle needs to be used to communicate with the LM5066 device through the PI Commander GUI, as shown below. The FTDI dongle comes with the LM5066EVK. Please order the LM5066EVK from the TI store. The USB2ANY…
Hi Ray,
Your setup connection is correct. It was mentioned in LM5066EVK. I think, setup connection figure is missing in LM5066i-EVM. I will take care to get it placed.
Best Regards,
Rakesh
Part Number: LM5066I Other Parts Discussed in Thread: LM5066EVK , I'm using the LM5066I for protection with UV at 24V, OV at 40V, and OC at 20A. I've got the circuit working on a dev kit, LM5066EVK/NOPB, having switched out parts to my FET and an LM5066I…