Part Number: LM5066H Hi sir,
When LM5066H fault event happen, how does it alert the system or MCU?
Can CRPS shut down LM5066H when fault happen by MCU/BMC? What's the fault event happen & shut down flow?
Thanks a lot!
Part Number: LM5066H Other Parts Discussed in Thread: LM5066 Hi, TI expert
The LM5066 and LM5066H appear to be pin-to-pin identical, except for the IMON pin (#27).
Please confirm if the LM5066 and LM5066H have identical specifications, excluding the…
Part Number: LM5066H Hi sir,
Because Nexperia and infineon have long L/T issue of their MOS products.
Could you help to ask your AE whether recommend other brand's MOS part number that the footprint are 5*6mm or 8*8mm or 10*10mm ?
Part Number: LM5066H Other Parts Discussed in Thread: LM5066 Dear Tier,
I would like to confirm the POWER LIMIT function, as shown in Picture 1.
During normal startup, does VDS < VPLIM_BL usually occur, and in that case, is high current operation…
Part Number: LM5066H Hi, I'm robotic enginneer in Korea.
Now, I'm trying to build Hot-swap system, and I have some questions about safety system.
I'll use 48V Lithium-ion battery, 30A rated current and 100A peak current (5seconds), Load capacitance…
Part Number: LM5066H Hi team,
The device's 100uA sourcing current capability means the block in the functional block diagram below correct?
2. The discription highlighted green is not correct. My customer thinks Vscp > Vsns > Vcb is correct…
Part Number: LM5066H
"When powering on the LM5066H1PWPR with a 24V input, the output ( 24V_sys ) initially ramps up but immediately falls back to 0 V. Attached are the schematic and oscilloscope waveforms for reference. Could you help explain what…
Part Number: LM5066H I am currently designing a hot-swap controller for my upcoming project. The key design parameters are as follows:
Input voltage: 55 V
Maximum load current: 20 A
The requirement is to implement a current blanking period of…
Part Number: LM5066H Hi sir,
My customer Portwell wants to evaluate LM5066H2 .
Could you pls provide below info?
sample and MP schedule
LM5066H2 EVM user guide, datasheet
Thanks a lot!
Part Number: LM5066H Hi,
I have questions about LM5066Hx ; how many fets could we use in parallel LM5066H1, would use of six parallel fets cause any issue on start up or fault shutdown?
Also could you please share the reference design for LM5066H1…