Part Number: LM5066I Tool/software: Hi there
We need digital hot swap controller with digitally configurable inrush controller. Can we use LM5066I for this application ?
Part Number: LM5066I Other Parts Discussed in Thread: TPS1685 Tool/software: Dear Team (TI)
I want to use LM5050-2 , LM5066I , Oring and Hot swap controller in my project, while designing system I have the following technical queries:
1. Can anyone…
Part Number: LM5066I Tool/software: Hi,
this is a follow-up of the previous post I made about some strange LM5066i telemetry behaviour.
It has been quite a while since then, but in the meantime I have received the LM5066i EVK. To be comparable to…
Part Number: LM5066I Other Parts Discussed in Thread: LM74502 Tool/software: Hello,
Is it possible to use the LM5066I for a 32V battery charge/discharge system?
Charge amperage less than 5Amps
Discharge 10Amps.
Thanks
H. E.
Part Number: LM5066I Tool/software: Hi Sir,
The LM5066I board that previously reviewed has now been manufactured. After performing the short circuit test, the LM5066I is showing abnormal behavior, with the GATE not functioning properly (VGATE = VOUT…
Part Number: LM5066I Other Parts Discussed in Thread: PMP23496 , LM5066 Tool/software: Hi TI experts,
Please review LM5066i schematics design based on 12V/266A, 3200W specification. You are confused why we used to high volage of input capacitors and…
Part Number: LM5066I Other Parts Discussed in Thread: LM25066 , Tool/software: Hi In the hardware circuit, the CL pin is floating, so according to the datasheet, CL = 50 mV. When CL=GND, READ_IIN => m=7645 * Rs; b=100.0; R=-2. I would like to ask, what…
Part Number: LM5066I Tool/software: It states in the datasheet that the LM5066I is for 10-80V Operation but the continuous absolute max is 100V. Can I use the IC on a system with 84V supply voltage?