Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: LM5066IEVM-626 Other Parts Discussed in Thread: LM5066I Tool/software: Hi Team
I am using LM5066I controller in our project for Hot-swap purpose. This controller has to be interface with SMBus of LM5066I and ARM processor (ARM Cortes operates…
Part Number: LM5066IEVM-626 Other Parts Discussed in Thread: LM5066I Hi. Based on the user manual, I should get a prompt to install the FT2232H Mini Module driver that connects to this EVB. I am not getting that prompt. Where can I install the specific…
Part Number: LM5066IEVM-626 Other Parts Discussed in Thread: LM5066I Hi Guys,
We need you help to check our customer's design.
Our customer would like to connect two LM5066IEVM-626 outputs parallel to being able to choose source of the power supply…
Part Number: LM5066IEVM-626 Other Parts Discussed in Thread: LM5066I Hello,
I am testing the LM5066IEVM-626 evaluation board.
I have some problems:
I configure for ILimit = 1.5A and in the load they are passing 3A. But I don't see that it limits the current…
Hi Rakesh,
Thank you for your support. Setting higher power limit solved the issue.
Could you provide information regarding maximum current sink capability of PGD and nSMBA pins?
I do not find any information in the datasheet regarding pin current sink…
Part Number: LM5066IEVM-626 Hi team,
My application specification as below.
1. Vin=Vout=43.2-52.8V
2. Iout_max=15A@48V
3. Load1=Back-DCDC(48Vto24V,Cin=200uF)
4. Load2=MotorDriver with Boost-DCDC(48Vto60V,Cin=440uF)
5.The loads are connected in parallel…
Part Number: LM5066IEVM-626 Other Parts Discussed in Thread: LM5066I , LM5066 Hi,
We seem to be experiencing some unexpected behaviour with the above part:
We have tied UVLO/EN to GND to ensure the mosfet defaults off when the device is powered up.
In…
Part Number: LM5066IEVM-626 Other Parts Discussed in Thread: LM5066 , LM5066I The PI-Commander software make error and closed application soon I select an LM5066 or LM5066I device. It works fine select other device(LM2506,LM25062,LM5056 ..).I installed all…
Part Number: LM5066I I have ordered 3 LM5066IEVM-626 Evaluation Modules directly from TI and none of them will communicate with my computer. Here are the issues that I have with this development platform;
The documentation is out of date; it references…