Part Number: LM5067 Tool/software: Hi
Please help to find the below thermal datas for the part LM5067MM-2/NOPB.
Max Allowed Tj (in degC)
RThetaJC
RThetaJB
RThetaJA
Thanks
Part Number: LM5067 Other Parts Discussed in Thread: LM5051 Tool/software: HI,
We need design support for UVLO, OVLO, Inrush current limit, Reverse Polarity protection using LM5067 IC or with any other suitable IC for Telecom application.
_Input rail…
Part Number: LM5067 Hi TI team,
can i use LM5067 in the low side switch application with operating voltage of 48V positive supply to the driver as shown in picture below:
Because in the LM5067 datasheet it is mentioned as -9 to -80V negative voltage…
Part Number: LM5067
Hi team,
I would like to ask you some questions or if you have detailed design manuals for this type of chip so that I can better understand the functions inside this chip.
1、What does the 1M resistor between the sense pin and…
Part Number: LM5067 Hello,team
I would like to consult about LM5067, the customer's current application is like this, VCC=5V, VEE=-48V, these two signals are not powered on together, in the first stage VCC=5V, VEE=0V; In the second stage is VCC=5V,…
Part Number: LM5067 Can the GATE pin of LM5067 drive two MOSs, as there may be some differences between the two MOSs? Will driving both MOSs simultaneously result in one switch being faster and the other being slower?
If this chip can drive, how does…
Part Number: LM5067 Tool/software: Hi Team
I have received an application notes of LM5067 from our supplier.
Since that application notes is written in Chinese, I am looking for English one.
Application Notes number is ZHCA812 released June 2018…
Part Number: LM5067 Tool/software: Hi Ti Team, Greetings! We like to know the Junction to Case (bottom) thermal resistance and Case Temp (°C) Max value of LM5067MM-2/NOPB.
Part Number: LM5067 hi expert,
lm5067 datasheet shows Fault detection current range is [140, 44] uA.
while another picture shows Fault detection current has little influence by temperature.
so above [140,44]uA range is mainly influence by…