Part Number: LM5069EVAL Tool/software: hi sir
I bought the LM5069EVB for LED tube control
we need the max power is 300w, but 230w limit
may i know which parameter need be adjust?
thanks
Part Number: LM5069EVAL Other Parts Discussed in Thread: LM5069 Hi team,
We are testing LM5069EVAL over current conditio but the action is not aligned with the pricinple as datasheet, pls help to check if it is normal:
Within the fault timeout period…
Part Number: LM5069EVAL Other Parts Discussed in Thread: LM5069 I'd like to ask some questions about the operation of LM5069EVAL(LM5069MMX-2/NOPB). We are currently using the evaluation board "LM5069EVAL" to verify the basic operation for product adoption…
Part Number: LM5069 Hi,
I have some issues with the LM5069 at 54 V while the circuit is working at 24 V. Can you help me ?
Here is the goal application:
First, I would to test the LM5069 with lower load power.
Here is the calculator…
Part Number: LM5069EVAL Other Parts Discussed in Thread: LM5066I , LM5069
I am looking for an Efuse for Vi> 80 to 100V (Viabs> = 100V); and CurrentLimit = 20 to 30 A. We have tested this component (LM5066I) but we prefer CurrentLimit to be hardware…
Part Number: LM5069EVAL Other Parts Discussed in Thread: LM5069 Hi Expert,
We are studying the LM5069 user guide (AN-1522).
It addressed the Q1 Power limit: 45W at beginning.
May we know why the user guide defined this 45W here.
Best regards…
Part Number: LM5069 I am trying to validate the functionality of the LM5069 chip using the evaluation board. I tested the board as is first, and reached the correct cutoff of 2.5A. I need a current limit of 9A, so I switched R5 to 5mOhms, but this resulted…
Part Number: LM5069EVAL Hi,
I have the LM5069EVAL evaluation board and I am using current limit to 10A (+28V).
I have a couple of question:
The insertion delay (in the LM5069EVAL) is 600ms – why? Can I change it to 200ms.
The restart time is…
Part Number: LM5069 I need to test the operation of an LM5069-1 part. I got the LM5069EVAL/NOPB board and swapped the LM5069-2 part that shipped with the board for an LM5069-1 part that was ordered at the same time. It needs to switch on at about 18.5V…
Other Parts Discussed in Thread: LM5069 , LM5069EVAL , TPS2493 , LM5060 I have a LM5069EVAL evaluation board that I am using to current limit a large capacitive load during startup (+48V). It takes a significant amount of time to charge the caps to 48V…