Part Number: LM5072 Dear Team,
Could you help to confirm the actual voltage range of LM5072 pin10, VCC According to the spec, it is 16V, but we actually tested it to 25V to make the LM5072 broken If we use 20V to supply power to VCC May I ask if the…
Part Number: LM5072 Hello PoE support team,
I have a problem that the MDI signal suffered from voltage spike issue.
Please refer to the picture below, during RJ45 signal line's plug/unplug, the MDI signal will occur the voltage spike during the transition…
Part Number: LM5072 I'm trying to retrofit an existing LM5072 circuit to use RAUX exclusively, meaning PoE will no longer be needed but the design should not be changed in principal.
We want to feed in 12-24V with a +-10% limit, meaning 10.8V-26.4V…
Part Number: LM5072 Hello,
We designed an output 12V/2A (24-watt) POE by using LM5072-80. We encounter a strange problem after change
the MOSFET (Q1 in our design). We have to change MOSFET, Q1 (APT55T10G), to other MOSFET ( SPN72T10T252TG )
due…
Part Number: LM5072 Other Parts Discussed in Thread: TPS23751 , PMP11254 Our POE 12V circuit refer LM5072 12Vout 25W PoE PD
http://www.ti.com.cn/cn/lit/ug/snvu100/snvu100.pdf
All component is same as the reference design. The output voltage is 7.3V…
Part Number: LM5072 Hello,
We have an 802.3at PD design by using LM5072-80. The design is a flyback design with output of 12V/2A.
It is working well with small output ripple (< 60mV) in static load. However, the output ripple is large than
1V when…
Part Number: LM5072 Other Parts Discussed in Thread: TPS23756 I need to fix up an existing PoE circuit to work with 12-24V external supply.
This should be theoretically easy, I figure I simply have to add a RAUX pullup to the new Vin. The circuit uses…
Part Number: LM5072 Hi, I used LM5072-80 as an isolated power for my board, which is in RAUX input mode and not for PoE application. Input voltage range is 18-72V and output is 3.3V. The schematic is almost the same as Figure32 in datasheet. But the 3…
Hi INg,
The LM5072 is not recommended for new projects as it is a non-standard 25W PD controller. What is their power (output voltage/current) and efficiency requirements? We can recommend a more suitable and optimized solution with out TPS237xx devices…