Part Number: LM5085-Q1 Greetings,
I am designing a power supply with 12V input using LM5085-Q1 chip. Nominal output for the power supply should be 9V, but also I would like to place a variable resistor in a feedback loop so I can change the output voltage…
Part Number: LM5085-Q1 Other Parts Discussed in Thread: LM5088-Q1 , LM5085 Hi,
I'd like to know if the automotive rated LM5085-Q1 has built in-load dump protection and fulfills the requirements set for ISO7637-2:2004[1] load dump pulse.
Taking for…
HI
some comments on layout:
1. below is LM5085 layout guildline, but in your layout, the first loop mentioned below is very large.
Two major current loops conduct currents which switch very fast, requiring the loops to be as small as possible to minimize…
Other Parts Discussed in Thread: LM5085-Q1LM5085-Q1 EMI test data for CISPR25
Do you have the EMI test data of LM5085-Q1 for CISPR25? My customer requires this data for reference. Could you share it to me if you have? Our customer's using condition is…
Other Parts Discussed in Thread: LM5085-Q1 Do you have the EMI test data of LM5085-Q1 for CISPR25?
My customer rwquires this data for reference. Could you share it to me if you have?
Our customer's using condition is the following,
Vin: 7V to 32V…
Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: LM5085 Hello guys,
One of my customers is trying to simulate LM5085 circuit using "LM5085 Transient Model" by Spice for TI for their new products.
They used a few of models (transistor…
7356.LM(2)5085_Quick_Start.xls
Hi Jimmy,
Here's the quick start calculator. It wouldn't let me change a several of the values, so it's not entirely complete. I will probe the SW node tomorrow.
Thank you,
-Alexander
Part Number: LM5085
I want to use the component as a current source during two modes. 1. continuous mode when we draw 0.2 A 2. flashing mode when we draw 5 A during a period of 1ms. Is IC responsive enough?
1. I simulated that, and the result matched…