Part Number: LM5088-Q1
While turning on the IC, there was a delay of 400ms observed between the Vin/VCC/EN pins and the voltage at the Css pin. This should not happen as there is no VCC UV and Standby Mode. Below are the attached waveforms for Vin, VCC…
Part Number: LM5088-Q1 Hey!
I am using LM5088QMHX-2 for generating 12V/5A output from 30V-60V input. Please find the attached schematic for the same.
I want to operate the IC at 143KHz. As per the TI WEBENCH, the Rt value is coming 44.2Kohm. And also…
Part Number: LM5088-Q1 Hi,
We designed a buck converter for our 802.3bt (71W) PoE application and used LM5088QMH-2/NOPB for it's wide input range after the PoE circuitry. The design is working fine, we got stable 16V output and we are getting around 4A…
Part Number: LM5088-Q1 We have used LM5088-Q1 to obtain 5V 5A and we have used the application circuit from the datasheet also values of the components has been selected from the suggested from the quick start calculator.
The output voltage is dropping…
Part Number: LM5088-Q1 Other Parts Discussed in Thread: LM5088 , Hello,
I'm posting on behalf of my customer. He is trying to do a design with the LM5088QMHX1, but it unable to simulate it. I tried using the default values and the same thing happened…
Part Number: LM5088-Q1 Other Parts Discussed in Thread: LM5088 , LM61460 part number: LM5088-Q1
Specs:
Input range: 9V - 36V
Output voltage: 5V
Max Load current: 5A
Switching frequency: 250KHz
The basic schematic is application schematic from the datasheet…
Part Number: LM5088-Q1 Other Parts Discussed in Thread: LM5088 Hello,
I am using LM5088-1 device in one of my project for the input range 30V - 60V and Output voltage 12V/5A. The basic schematic is generated using the Webench Power design tool for the…
Part Number: LM5088-Q1 Hi TI-team
My customer has question.
Although the gate of the external FET is connected to the HG pin (pin 14), ringing occurs in the operating waveform.
It will be improved by adding a gate resistance between the HG pin (pin 14…
Part Number: LM5088-Q1 Other Parts Discussed in Thread: LM5088 Tool/software: WEBENCH® Design Tools Hi sir,
I have created a design using the LM5088 by WEBENCH.
Vin =5V , Vout = -60V, Iout =100mA.
The following are the parameters setting and schematic…
Part Number: LM5088-Q1 Hello,
Client using LM5088-Q1 in his power supply project - Vin=13-70V, Vout=12V@3A.
During testing the IC & MOSFET burn down if Vin > 52V is applied. This happens with no load and 1A load. What might be the cause? Could this…