Part Number: LM5088-Q1 Tool/software: WEBENCH® Design Tools Hello. I am designing a power supply circuit with an operating voltage range of 18-65 volts and a current limit of 7 amperes on the LM5088-1 microcircuit. I assembled a printed circuit board…
Part Number: LM5088-Q1 Other Parts Discussed in Thread: LM5088 , LM5116 , LM5145 , LM5146-Q1 Tool/software: WEBENCH® Design Tools So im in the process of creating a DC/DC converter.
INPUT 48V (10A possible)
OUTPUT 19.5V 10A
Im in the early phase and have…
Part Number: LM5088-Q1 Hi Team
D/S says the bottom feedabck resistor(Rfb1) sould be selected by the current through the resistor (1.2V/Rfb1) is in between 1mA and 100uA.
my question is ..
[1] why we set Max 1mA ?
[2] why we set Min 100uA ?
Part Number: LM5088-Q1 Other Parts Discussed in Thread: LM5088 , CSD19534Q5A
We are testing LM 5088 based buck converter,
Input voltage: 48V
Output: 12V
Output current 5A
Switching frequency: 500Khz
Diode Part number: Digikey V40PW10C-M3/IGICT-ND
Mosfet…
Part Number: LM5088-Q1 Other Parts Discussed in Thread: LM5088 When we were testing LM5088 there was too much ringing in mosfet gate and switching node. We tried adding snubber, adding capacitor close to mosfet but none of that doesn't helps. Not sure…
Part Number: LM5088-Q1 Other Parts Discussed in Thread: LM5088 Tool/software: WEBENCH® Design Tools Hi Team,
We simulated LM5088-Q1 using WEBENCH.
(Please refer to the URL)
https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=72E7F0392361BAF1
…
Part Number: LM5088-Q1 Other Parts Discussed in Thread: LM5088 LM5088 input 15V 60V voltage and 5V10A output. At present, it is found that the output 5V voltage is normal, the output voltage can not be loaded, and the on-load output voltage drops to 0…
Part Number: LM5088-Q1 Other Parts Discussed in Thread: LM5088 Hello Sir,
is IC LM5088 can be used for variable output application?
is it possible to change the output voltage by changing the resistance of voltage divider circuit?
Part Number: LM5088-Q1
Tool/software: WEBENCH® Design Tools
Hello TI Webbench developers,
I would like to report some issues to the Webbench EAGLE export feature, because in the current form it is hardly usable.
I would suggest to merge the SCH and…