Part Number: UCC27282 Other Parts Discussed in Thread: LM5101C , UCC27211 , UCC27211A , LM5101A , UCC27288 , UCC27301A-Q1 Dear all,
Background:
My customer now are designing a 4 switched Buck-Boost converter. And they are using UCC27282 as the gate…
Hey Nison,
Thank you for reaching out regarding the mechanical information for the UCC27212.
We have recently released a revision for this datasheet and during the release process the mechanical data was not properly added to the datasheet. We are…
Hi, Hui,
The LM5101 isn't recommended for new designs. There is an LM5101A which is recommended, and has a model. You can use the model in the LM5101A web page for either device, though.
Another alternative is one of our newer devices, UCC27282 which…
Hello Cheney,
As you have likely seen from the datasheets the LM5101A and UCC27201 are similar half bridge drivers with 100V HS voltage rating and 3A drive current.
The differences are mainly in two areas. The VDD rating of the UCC27201 recommended…
Part Number: LM5100A Other Parts Discussed in Thread: CSD88539ND , , LM5101A When using the LM5100AM Gate Driver according to the typical application circuit shown in the data sheet, LO and HO signals when probed do not show the expected outputs. I believe…
Part Number: LM5100A Other Parts Discussed in Thread: LM5101A , UCC27289 , UCC27282 , UCC27284 Hi TI expert
May I know if LM5100A could directly connect 3.3V CMOS?
Is TTL compatible with CMOS ?
Best regards,
Thomas
Hello Viabhav,
If you are running simulations, you can find the simulation models in the LM5101A product folder which should have the TTL compatible inputs.
Please confirm if this addresses your question, or you can post additional questions on this…
Part Number: LM5106 Other Parts Discussed in Thread: LM5101A , UCC27712 , TPS28225 , TPS51604 , LM5101B , LM5102 Hi,
my customer is using LM5106 and the drive current is small. They need at least 2A drive current, so I propose LM5101A/B, but this part…
Hello Glenn,
I am with the high power drivers application team, and have reviewed the schematic sent thru a private channel from Rick.
I do have some comments and suggestions. I think Rick mentioned comments about C8, C10 and C9 values, and I agree…
Hello Parth,
Thank you for your interests in the TPS61086. From you description, what you need is actually a half-bridge driver that the mps430 can control to operate in the boost mode. Please consider LM5101A or something similar. Also, the TPS61086…