Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Other Parts Discussed in Thread: LM5102 , LM5105 Hi
my customer wants to reach 50ns dead time on LM5105 / LM5102.
our D/S says that deadtime can be adjusted from 100ns to 600ns which seems to tell that 50ns is not achievable
BUT
it also says that one can…
I have been asked to look into this query.
Could you please remove BOTH the Upper and Lower MOSFETs and re-measure the voltage on the HS pin of the driver wrt VSS ? Please also remove the 57.6K resistor between the motor node and VSS. Lets get the MOSFETs…
I am using LM5105SD - half bridge MOSFET controller in my design. The device was subjected to failure, observed by a low impedance path across Vdd and Vss power rail. It was also observed that IC which has failed, reads a low impedance of 12 ohms across…
Other Parts Discussed in Thread: LM5105 What is the highest switching frequency that LM5105 can work at? Can LM5105 work at 1MHz switching frequency? Thanks.
Other Parts Discussed in Thread: LM5105 For a class-D power stage, I am using the LM5105 to drive Vishay power MOSFETs. The circuit is as simple as the setup shown in Figure 24 of the datasheet. During circuit qualification, I have been facing the following…
Other Parts Discussed in Thread: LM5105 , LM5102 In comparing the datasheets for the LM5100/LM5101x with the datasheets for the LM5102 and LM5105, there is roughly a factor of 3.5x increase in boot-strap diode dissipation for the 02 and 05 parts for similar…
Other Parts Discussed in Thread: LMG1210 , LM5106 , LM5105 , LM5104 , UCC27710 , UCC27712 , TPS28225-Q1 , UCC27712-Q1 FAQ: How to use a dual input half-bridge driver with a single PWM signal
An easy way to convert a half-bridge driver with dual inputs to work…
Other Parts Discussed in Thread: LM5105 , LM5101 I am looking for a Half bridge gate driver with the following specs.
-Operate at 28VDC.
-Output 500mA
-Can be configured as high impedance.
-Switching speed less then 200ns.
I found the LM5105 that will meet…
Part Number: LM5104 Other Parts Discussed in Thread: LM5106 , LM5105 Dear TI team,
Good morning.
Do LM5104 and LM5106 support high frequency of 2 Mega Hz ?
kindly reply.
Thank you,
Caliber