Other Parts Discussed in Thread: LM5107 Hi Team, I looked Layout Guidelines and have following questions. question 1) Could you tell me the recommended value of the capacitor that should be connected between VDD and VSS? I would also like to know the value of…
Other Parts Discussed in Thread: LM5107 Hi TI,
I need your help. Can you give me the true table for LM5107? The true table should include HI, LI, HO, LO.
Thanks,
Don
Other Parts Discussed in Thread: LM5107 Hello
I intend to use the LM5107 in a new design. The circuit topology is relatively straightforward, or so it seems.
I'm looking to swing the common node (source of Q1, drain of Q2) at low frequency from the DC bias…
Other Parts Discussed in Thread: LM5107 Hello
I intend to use the LM5107 in a new design. The circuit topology is relatively straightforward, or so it seems.
I'm looking to swing the common node (source of Q1, drain of Q2) at low frequency from the DC bias…
Other Parts Discussed in Thread: LM5107 Hi,
What charge is required by the internal level shifter for LM5107?
Needed to calculate needed bootstrap capacitance.
BR/
Mats
Other Parts Discussed in Thread: LM5107 Hi
LM5107 has internal bootstrap diode.
but there is not detail spec in LM5107 datasheet.
please let me know that like below picture. my e-mail is dexter.choi@avnet.com
Daniel ,
I do not answer one of your questions , which is , what frequency EMI EMC Test Done?
1.) It is 20MHz - 2Ghz, Could you please suggest , if my Pcb with Lm5107 or Lm5164 Will pass t EMiEMC Test?
Rohit
Part Number: LM5033 Other Parts Discussed in Thread: LM5107 , LM5030 I have a customer using the LM5033/LM5107 in a similar implementation as shown in the Datasheet (Figure 11); only the system has 24V input and 12V output.
They have a test criteria that…