Part Number: LM5109B Other Parts Discussed in Thread: LM5109 Hello,
checking the MPPT charge controller reference design for 12- and 24-V solar panels a RC filter has been added between the mcu and LM5109.
Is this RC (or only R) suggested when a 3…
Part Number: LM5109B Hi,
I'm using this gate driver to control a half bridge contains two N-MOSFET, my MOSFET is powered by 36V, so my HO should be at least 46V to totally turn the MOSFET at on state, besides, my LO should be 12V. I don't understand…
Part Number: LM5109B Other Parts Discussed in Thread: UCC21220 Hi,
We are using LM5109BMA/NOPB for BLDC motor driving application. The Motor is 60V/5A rated.
We are using three LM5109BMA/NOPB chips to drive three half bridges.
We are facing high…
Bjornar,
LM5109B has an increased UVLO functionality that holds the high side FET off when the main VDD supply voltage falls before the HB (bootstrap) voltage decays. The relevant tables are found in the LM5109B's datasheet, in the Start-Up and UVLO…
Part Number: LM5109B Other Parts Discussed in Thread: LM5109 Hi,
I have LM5109B and i want to select MOSFET for this.What is maximum rating of MOSFET gate charge(Qg) as i want to drive MOSFET through LM5109B.
Can i connect MOSFET with Qg=400nC on…
Part Number: LM5109B
Please go through attached schematic in which LM5109BMA/NOPB is used as gate driver for Three-Phase bridge.IRF530PBF is used as MOSFET Switch.
PCB-BLDCDRVR-1918-1B-01.pdf
Problem Definition: Supply Get Shorted while applying…
Part Number: LM5109B Other Parts Discussed in Thread: CSD19534KCS
Hi,
We are using LM5109B with IRF3415 mosfets to drive a BLDC.
Without connecting the BLDC when we increase the inverter supply above 18VDC the supply gets short circuit.
After…
Part Number: LM5109
There have been questions regarding the differences between the LM5109A and LM5109B 100V high-side low-side drivers.
The pinout, available packages and parameter specifications are the same for the LM5109A and LM5109B. So the LM5109B…
Part Number: LM5109B Hello Team,
Even if power is supplied to HB in ten or more seconds after power input to VDD, is there a problem with device?
Best regards, Kato