Part Number: LM5110 Tool/software: Hi All,
Kindly refer the below input and suggest me a solution please.
For a design I require to generate a pulsed output of level "0V & -10V" at a max of 25 MHz.
This pulsed output has to controlled…
Part Number: LM5110 Hello,
What is the maximum rating for the OUT_A and OUT_B pins of the LM5110-2? Please tell me the MIN and MAX. There is no description in the data sheet.
Best regards,
Part Number: LM5110 Hi all,
For MRL analyses I would like to know the DIE size for the component reference LM5110-1SDNOPB ou LM5110-1SDXNOPB. Is it possible to have this information ?
Best regards
Philippe SYLVAIN
Part Number: LM5110 Other Parts Discussed in Thread: LM5111
Hi Team,
LM5110-3M is composed by Inverting “A” OUTPUT and Noninverting “B” OUTPUT.
During UVLO mode what is the logic of output “A” and “B”, all the…
Part Number: LM5110 Other Parts Discussed in Thread: UCC27524 I need clarification on the LM5110-1M/NOPB gate driver.
The LM5110 datasheet does not mention the part’s drive strength pulling ‘Low’ when the SHDN pin is low . I’m guessing…
Part Number: LM5110 Other Parts Discussed in Thread: UCC27525 While entering in my question, I saw the problem. So I'm really asking for a potential part or solution.
The LM5110 datasheet only refers to driving N-CH MOSFETS.
I wanted to use the LM5110…
Part Number: LM5110 Hi All,
In the LM5110 datasheet, it says that pins 5 and 6 of the DPR package are "Not Connect". The term "Not Connect" does not tell me that I must leave the pin floating ("Do Not Connect") or that I could tie it to GND or any other…
Part Number: LM5110 hi, I'm a FAE of TI, My customer has a question about LM5110
from the Datasheet, we can know that the maximum input voltage level of LM5110's IN_A and IN_B pin is "IN to IN_REF -0.3-15V"
so we just need to consider…
Part Number: LM5110 Would you please advise if clamping body diodes are present on the OUT_A and OUT_B pins? i.e. if the device is unpowered will the outputs be clamped to a diode drop from 0V?
Thanks