Part Number: LM5112-Q1 Hello,
On a DCDC converter we use LM5112Q1SD for drive the MOSFET bridge and it is work perfecly.
Before assembling the product, we test each board with flying prob and we measure the output impedance of the driver (OUT pin / VEE…
Part Number: LM5112 Hello,
May I to know what this step works for?Is it good for solder reflow soldering?
Looking forward to your reply,thanks.
best regards!
Miss Yang
Nov.10.2022
Other Parts Discussed in Thread: LM5112 , UCC21225A Hello,
I wonder if TI provides IBIS model of gate drivers, LM5112/UCC21225A/27201/27282/27324/27524A. It doesn't look it's provided if the device doesn't have PMbus/I2C communication functionality, though…
Part Number: LM5112-Q1 Hi
in case a voltage applied on the input pin trough 20K pull up resistor before VDD is supplied to the IC.
Can it cause a latch-up? the current is very low ~0.15uA
or any other issue with the IC?
Part Number: LM5112-Q1 Other Parts Discussed in Thread: LM5112 , TINA-TI hi
I am trying to use LM5112 spice model in Keysight ADS but it sais it has a syntax error.
I read in one of the threads here that it is due to bad translation off switch models in…
Part Number: LM5112 I am working on a design using the LM5112 on a dual-supply (+6 and -8V) application. I would like to connect the IN_REF pin to ground to allow for simple TTL control. The recommended operating conditions specify that VCC to IN_REF…
Part Number: LM5112 Other Parts Discussed in Thread: LMG1020 , UCC27611 , CSD17381F4 , LMG1205 , LMG1210 Dear All,
i need to pulsed an uv-led with a frequency from 100kHz ( 5 us on, 5 us off) to 1 MHz ( 500ns on 500ns off) with few ns of rise/fall time. I…
Part Number: LMG1210 Other Parts Discussed in Thread: LM5112 Dear TI-development team, i am currently writing my bachelor thesis and would like to use the LMG1210 to control a switching amplifier in the half-bridge topology. Since I would like to utilise…