Part Number: LM5113-Q1 Tool/software: Hello team - the datasheet and TI packaging website both refer to a product data sheet for the packaging information on the 10-pin DPR WSON package. "This image is a representation of the package family, actual package…
Hi Kazukhi,
LM5113-Q1 and UCC27302-Q1 have different spec and are offered in different packages. Selection between these two depends on type of switch that requires the driver, LM5113-Q1 is mainly used to drive GaN FET and UCC27302-Q1 is used to drive…
Part Number: LM5113-Q1 Other Parts Discussed in Thread: LMG1205 , LMG1210 , Right now, we are developing the new controller. We are looking for single GAN FET for replacement of back-to-back N-channel MOSFET. The back-to-back N-channel MOSFETs are used…
Part Number: LM5113-Q1
Tool/software:
When using the LM5113-Q1 I cant seem to get my bootstrap working. It works for a short while in the beginning of the pulse but then just stops. Below is the circuit I use. It might not be that visible but VSS…
Part Number: LM5113-Q1
Hi, I'm Takamoto Furuichi, DENSO Corp.
We would like to ask about the fluctuation of the charactoristics due to the external stress.
If you have the data of "turn on propagation deley" vs "external stress" or " turn on propagation…
Part Number: LM5113-Q1 Other Parts Discussed in Thread: LMG1025-Q1 ■ Target: LM5113-Q1, LMG1025-Q1 ■ Desired data: Temperature characteristics of propagation delay time ⇒Propagation delay time at -40, 25, 150℃ and its variation. In addition, I would…
Part Number: LM5113-Q1 Other Parts Discussed in Thread: LM5113 The driver is being used as an independent high and low-side MOSFET driver.
The high side charges 1300uF of capacitive load, and its use is for inrush current limit. That means that HS…
Part Number: LM5113-Q1 Other Parts Discussed in Thread: LM5113 , UCC27624 , LMG1205 , LMG1025-Q1 Hi, I'm Takamoto Furuichi, DENSO Corp.
I have the question about the LM5113's spec.
We have confirmed that the following turnon delays tend to depend…
Part Number: LM5113-Q1 Other Parts Discussed in Thread: LM5113
My question is on the
Lm5113 part , the Tmon and Tmoff shows a delay matching of 1.5ns typical max 8ns I have a few questions
What is the output impedance of the driver during…