Other Parts Discussed in Thread: LM5025 , LM5115 Hello,
One of our customers is planning to use the LM5025 and they want to use the output inductor secondary windings to connect 2*LM5115
The output of the Inductor on the secondary will provide the working voltage…
Part Number: LM5155 Other Parts Discussed in Thread: LM5115 Hi,
How are tr and tf calculated on the following calculator?
We would like to know to check equation(33).
Best Regards,
Kuramochi
Part Number: LM25118 Other Parts Discussed in Thread: LM5155 , LM5115 , LM2775 Hii Team .
Please find attached the Image for review.
Scheme 1:
Input voltage (Battery charger output ): 3.2V to 4.2V
Output voltage: 4V
Output current: 6A
Hi, Scott,
Lots of TI power management ICs have the external sync capability. For example, LM5115, it has sync pin directly interface with the external signal.
www.ti.com/.../lm5115.pdf
Or some UCC part, like UCC28C43, you can modify the its sawtooth…