Part Number: LM5116-HT Other Parts Discussed in Thread: LM5116WG Hi
I am evaluating LM5116-HT and LM5116WG for high temperature, high voltage power supply design. The target working voltage is above 60V and temperature of around 175C.
At room temperature…
Other Parts Discussed in Thread: LM5116-HT , LM5116 hello
Does TI provide the Spice model of LM5116-HT for Thermal simulation prupose?
I am planning to use it at 150C for 48V/4A application. Is this achievable by LM5116-HT buck converter?
Thanks for…
Other Parts Discussed in Thread: LM5116-HT Thanks Nikhil for the response.
Is that alright for TI provide us the technical information whether the LM5116-HT able to supply 200Watt at 150C? If not, what is the maximum output power LM5116-HT?
Thanks. …
Hi Daniel, good day,
I've tried to reduce the inductor to 22uH, and the the value of oscillating load current will move to about 0.5A.
I'm interested in the cause of this oscillation. The oscillation occurs when the inductor current is critical continuous…
Part Number: LM5116 Hi,
The LM5116 is rated for Vin =100V and an operating temperature range of -40°C to 125°C. I am looking for operation down to -55°C.
I found the LM5116-HT, which expands the range to -55°C to 175°C, but also lowers Vin…
Other Parts Discussed in Thread: LM5116WG , LM5116 , LM5116-HT , LM5141 , LM5119 I am looking for a buck controller with synchronous rectification, current mode and external MOSFETs to be used for a VIN=37 to 58.8V power supply with 15V output and also a power…
Other Parts Discussed in Thread: LM5116-HT I have designed a DC-DC buck power supply with a LM5116-HT. I am attaching the schematic, PCB layout file(Both are in Altium) and the Gerbers.
I am having issues with the following issues with the power supply…