Part Number: LM5118 Other Parts Discussed in Thread: LM5177 Tool/software: Dear TI Engineer,
Our requirement is to achieve the input of 9V to 55V, output of 24V/6A and 24V/12A. We have noticed that LM5118 is a buck-boost controller product, but on…
Part Number: LM5118 Tool/software: THIS IS MY LM5118 buck boost converter circuit .my problem is it will not give 12v output if i given 10 v from J3 but it will give only 3v LM5118 DRAFT.pdf or 5 volt only and also get more amps like 0.01A .could you…
Part Number: LM5118 Hi expert TI....
My regulator does not work when I try to start it with the load set to my minimum input voltage (12 Vdc), I have to add a delay to the load to wait for it to work. How can I get around this?
VOUT = 12 VDC VIN…
Part Number: LM5118 Tool/software: Hi, I would like generate a 24Vdc/120W with 12-100V input voltage. So, i think about the LM5118 but its max input voltage is 75V. Do you think I can separate power supplies? - to reduce the maximum voltage, i can use…
Part Number: LM5118-Q1 Other Parts Discussed in Thread: LM5118 Hi,
I need to design the input filter for the LM5118, I was referring to the app. note snva538. Under the Appendix example calculations, DC resistance Rl = 0.088 ohm, How did they get the…
Part Number: LM5118 Other Parts Discussed in Thread: CSD13202Q2 Tool/software: I have used TI Webench Power designer for design help of generating 9V @1A using a 3.7V battery and LM5118MH/NOPB Regulator. When we tested the PCB, The IC (LM5118MH/NOPB)…
Part Number: LM5118-Q1 Hi Team,
I have design 9-36Vin to 24Vout @3A power supply using Lm5118-Q1 IC, I have used the components value recommended by Webench design for the same. Everything is working fine. but during short circuit test I am still getting…
Part Number: LM5118 Hello.
We are working on a webench design LM5118MH design and are having issues getting the switcher to run. It is 12V - 30VDC in to 24V @ 3A output without any changes except some higher voltage values on caps. The switcher is holding…
Part Number: LM5118 Hello,
I am designing a converter with LM5118. In this process, I follow the typical application in the datasheet. However, I noticed some errors in the calculations and I would like to both report and confirm them.
The first error…
Part Number: LM5118 Tool/software: I have some customers that are returning boards with a dead main switcher (LM5118, 10-36V input, 12V output @~4A max). The design has been rock solid for years, but a few have come back recently and we are just replacing…