Part Number: LM5118-Q1 Other Parts Discussed in Thread: LM5177 Real-time output control
I'm trying to design a Non-Inverting Buck-Boost (NIBB) power stage using TI controller LM5118-Q1. The issue I deal with is the requirement for controlling many…
Part Number: LM5118-Q1 Other Parts Discussed in Thread: LM5118 Hi,
LM5118 is designed for converting the input voltage (6-70) to 12V @3.5A output using the webench power designer.
The contactor coil voltage is 12V and the max inrush current is 3A , it…
Part Number: LM5118-Q1 Other Parts Discussed in Thread: LM5118 When I test EN threshold of LM5118,I find that the EN Input High Threshold is 1.7V,the low threshold is 1V。
However the EN Input High Threshold is 3V ,the low threshold is 0.5V in datasheet. …
Part Number: LM5118-Q1 Other Parts Discussed in Thread: LM5118 , , LM5113 Hi Sir,
My customer is developing a board to refer the 4 switch design of LM5118 for 4.2~60V-in to 14V-out with 10A output current.
In the boost mode, they would like to test the…
Part Number: LM5118-Q1 Other Parts Discussed in Thread: LM5118 Hello Team,
I am using LM5118-Q1
Having following load requirements
Input Voltage Range: 6V to 32V
Output Voltage : 5V ± 3% tol
Expected Load current: 1.5Amps
Regulator meets above…
Part Number: LM5118-Q1 Hello,
Our application requirement are given below:
Input voltage range: 6V to 36V
Output voltage: 5V
Load current: 1.5A
Background:
We are using the above mentioned product in one of our project. We were using it with switching…
Part Number: LM5118-Q1 Hi team,
Could you help confirm the R3 calculation? If Vinmin is 5V and R1 is 75kohm, R3 should be around 22kohm, not 29kohm.
Regards,
Dongbao
Part Number: LM5118-Q1 Other Parts Discussed in Thread: LM5118 Hello,
I have used LM5118 for a buck boost converter design in LTSpice with unencrypted model available in the TI website and i have the following issues appear in the error log
could you…
Part Number: LM5118
Hi,
I am trying to design a Power Board Supply with the LM5118 that will output 24V 2A that is then further connected to a 12V (OKI-78SR-12/1.0-W36-C) & 6V regulator (L7806CV-DG).
I have two problems:
1. When I start up the from…
Part Number: LM5118-Q1 Other Parts Discussed in Thread: LM5118 Hi,
Please find the attached, schematic and layout of the design which is using LM5118-Q1.
Input voltage - 10VAC to 50VAC, Output = 25V/2A
The PCB is 4-layer with Signal-GND-Power-Signal stack…