Part Number: LM5118-Q1 Tool/software: WEBENCH® Design Tools Hello,
I created a design using the LM5118-Q1 in Webench. My input parameters were as follows:
Vin Range - 10.5 to 36V
Iout Max - 3A
Link to design: https://webench.ti.com/appinfo/webench/scripts…
Part Number: LM5118-Q1 Other Parts Discussed in Thread: LM5118 , LM5088 the attachment is the schematic used lm5118&lm5088, please help to review and give your comments if have any problem, thank you
LM5088-5188.pdf
Part Number: LM5118-Q1 Hello Team,
What is the maximum propagation delay of LM5118-Q1 to start up the output voltage after EN is in high state?
Please provide the relevant data on the T_en as marked in the diagram below.
Best regards, DY
Part Number: LM5118-Q1 Other Parts Discussed in Thread: LM5118 , LM5141 , PMP15041 , TPS54360 Hi Team,
I am using LM5118-Q1 BUCK-BOOST controller.In NO load condition its will take 5 to 7mA.i need Operating Quiescent Current is less than 500uA.kindly give…
Part Number: LM5118-Q1 Other Parts Discussed in Thread: LM5118 Dear TI Team,
I am designing the LM5118-Q1.
We design a 5V 1A output on 4 ~ 8V inputs.
The LM5118-Q1's data sheet contains the phrase 5-V VIN is required to initially start the controller…
Part Number: LM5118-Q1 Hello, After revising my layout design due to prior advice, I have built a prototype and have begun testing it.
I have found that it functions in buck mode, where the input supply is greater than the output, but does not function…
Part Number: LM5118-Q1 Other Parts Discussed in Thread: LM5118 Hello, I am having difficulty getting a 24VDC to 24VDC regulator working using the LM5118-Q1. It is to protect some equipment in an industrial automotive environment. The specs I hope to achieve…
Part Number: LM5118-Q1 HI,
For LM5118Q1MH, VIN = 15 - 30V, VOUT = 21.5V, Load = 3.0A. Our voltage output test fails on some production units when VIN = 27.25V-27.75V (.25V per test step). When we analyze it appears that the suspect devices are switching…
Part Number: LM5118-Q1 Other Parts Discussed in Thread: LM5118 Good Day,
I have the controller set at 14 V, 300 kHz, 123 ms of soft start, undervoltage threshold at 4.5 V.
The input voltage comes from a generator that outputs a rectified dc voltage of…